Can't init device hci0: Connection timed out (110)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't init device hci0: Connection timed out (110)

1,354 次查看
Ashwini_A
Contributor I

I'm am working with imx93 board in Linux 6.6.52

I have used below  commands to enable BT interfcae

modprobe moal mod_para=nxp/wifi_mod_para.conf
modprobe btnxpuart

hciconfig hci0 up
Can't init device hci0: Connection timed out (110)
and Im getting error like this
BT module name -LBEE5PL2DL-921

1 回复

1,338 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Is there any error message during the boot up? Is the driver loading correct?

e.g. is the path of the firmware incorrect? are the gpio pins for controlling the chip is properly?  

What is the setup in your board device tree?