Can't Program or Enter Debug Mode on a MC9S08QE32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't Program or Enter Debug Mode on a MC9S08QE32

跳至解决方案
1,474 次查看
Designer11
Contributor IV

Hi Guys,

 

I'm desperately needing your help on this issue. I designed a board with a QE32 uController and every time I used either the USB multilink or Multilink Universal I can't program the board or get the board to enter debug mode. The two Multilinks work great with the QG8 series.

 

On the other hand, when I use the cyclone Pro with the board it enters debug mode and able to program the board without any problem. What I did for a test was I toggle a port on the MCU.

 

BR,

标签 (1)
0 项奖励
回复
1 解答
1,026 次查看
Designer11
Contributor IV

I don't know why the QE32 microcontroller required the VDD Line to connect to the programming header, even if you are not using the Vdd voltage on the programmer header to power the target board.  But You have to connect it from the target board to your Multilink programmer,

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,027 次查看
Designer11
Contributor IV

I don't know why the QE32 microcontroller required the VDD Line to connect to the programming header, even if you are not using the Vdd voltage on the programmer header to power the target board.  But You have to connect it from the target board to your Multilink programmer,

0 项奖励
回复
1,026 次查看
kef
Specialist I

Multilink is multivoltage tool. Since Vdd range is as big as 5 to 2.7V or even less, you need to provide your target Vdd to Multilink to make it able to convert logic levels to internal Multilink levels properly.

0 项奖励
回复
1,026 次查看
Designer11
Contributor IV

Kef,

 

Thanks for the explanation.

 

BR,

D

0 项奖励
回复