Can't Program or Enter Debug Mode on a MC9S08QE32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't Program or Enter Debug Mode on a MC9S08QE32

Jump to solution
2,436 Views
Designer11
Contributor IV

Hi Guys,

 

I'm desperately needing your help on this issue. I designed a board with a QE32 uController and every time I used either the USB multilink or Multilink Universal I can't program the board or get the board to enter debug mode. The two Multilinks work great with the QG8 series.

 

On the other hand, when I use the cyclone Pro with the board it enters debug mode and able to program the board without any problem. What I did for a test was I toggle a port on the MCU.

 

BR,

D 

Labels (1)
0 Kudos
Reply
1 Solution
1,988 Views
Designer11
Contributor IV

I don't know why the QE32 microcontroller required the VDD Line to connect to the programming header, even if you are not using the Vdd voltage on the programmer header to power the target board.  But You have to connect it from the target board to your Multilink programmer,

View solution in original post

0 Kudos
Reply
3 Replies
1,989 Views
Designer11
Contributor IV

I don't know why the QE32 microcontroller required the VDD Line to connect to the programming header, even if you are not using the Vdd voltage on the programmer header to power the target board.  But You have to connect it from the target board to your Multilink programmer,

0 Kudos
Reply
1,988 Views
kef
Specialist I

Multilink is multivoltage tool. Since Vdd range is as big as 5 to 2.7V or even less, you need to provide your target Vdd to Multilink to make it able to convert logic levels to internal Multilink levels properly.

0 Kudos
Reply
1,988 Views
Designer11
Contributor IV

Kef,

 

Thanks for the explanation.

 

BR,

D

0 Kudos
Reply