CW for HCS08 V.5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW for HCS08 V.5.1

2,332 Views
Truk
Contributor I
New source Files.
If I take "NEW TEXT FILE" and store the file with extension xx.A08 the file shows the defined colors - in my opinion - it is accepted as a source file.
The problem is that the new files will not be shown in the project window in the source file group.
I have tried with
MAKE
FIND AND OPEN File
to solve this problem but I had no success
 
How have I to do this?
Truk
 
 
Labels (1)
0 Kudos
Reply
1 Reply

1,506 Views
alex_spotw
Contributor III
Hi:

You have to RIGHT click on the source file group, and then select the ADD FILES option, which opens a dialog window where you can browse and select the files to add.

Regards,

Alex
0 Kudos
Reply