CAN tranceiver problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN tranceiver problem

ソリューションへジャンプ
2,483件の閲覧回数
binukannur
Contributor III

Hai,

     Iam using freescale DSC controller for automotive application.Using this, I want to use CAN communication. So I used can tranceiver LT1796(http://cds.linear.com/docs/en/datasheet/1796f.pdf)) .

But problem is,  controller is in 3.3v logic level but LTC tranceiver is in 5v operation.

In S08 controller it works fine with this CAN tranceiver.

Can I use 3.3v controller with 5v CAN tranceiver?

If not please suggest a tranceiver IC.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,179件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello,

Provided you adhere to the DC Electrical Characteristics mentioned on the datasheet, I do not see a problem using the LT1796 transceiver.

Please be aware of the following information:

parameteres.JPG

If the microcontroller can supply the TXD signal with the features needed for the LT1796 transceiver, your application should work correctly.

In order to get more information about the CAN transceivers from Freescale, please refer to the following link:

Controller Area Network (CAN)|Freescale

can transceiver.JPG

Hope this information will be useful for you.

Have a great day.

David

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,180件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello,

Provided you adhere to the DC Electrical Characteristics mentioned on the datasheet, I do not see a problem using the LT1796 transceiver.

Please be aware of the following information:

parameteres.JPG

If the microcontroller can supply the TXD signal with the features needed for the LT1796 transceiver, your application should work correctly.

In order to get more information about the CAN transceivers from Freescale, please refer to the following link:

Controller Area Network (CAN)|Freescale

can transceiver.JPG

Hope this information will be useful for you.

Have a great day.

David

0 件の賞賛
返信
2,179件の閲覧回数
binukannur
Contributor III

Thanks David,

    It works fine. The problem is in my hardware side. I remove the pullup resister that Iam already did.

0 件の賞賛
返信