Hello All,
Have a problem with a short assembly language program
running on a M98S08AC32-64
CodeWarrior is killing me by throwing errors on what looks like legit code.
Thank you all,
Code is below.
Randall
Doofus(void) {
asm {
brclr 6,cmdsave,scan_2
brclr 6,soundop,scan_11
brset 6,command,scan
}
}
CodeWarrior 6.2
Throwing unknown opcode 45. It does this with TAX and other instructions
Hello Randall,
The BRSET and BRCLR instructions are applicable to a page zero location only. Therefore, your cmdsave, soundop and command variables will need to be explicitly allocated to Z_RAM segment. Additionally, the branch addresses scan_2, scan_11 and scan require to be within range for relative addressing mode.
I cannot comment about your TAX problem without knowing the context.
Regards,
Mac
MAC,
Worked perfectly, moving things into zero page with the #pragma worked. Thanks to you all.![]()
Having another crazy problem, the code below is a small project that results in an error C18000
Label not set, however, as you can see the label clearly is set. Am I having another zero page error here?
Thanks, Randall.
#include <hidef.h> /* for EnableInterrupts macro */
#include "derivative.h" /* include peripheral declarations */
// memvar declarations
#pragma DATA_SEG __SHORT_SEG MY_ZEROPAGE
char flag1 = 0x01;
char soundop = 0xFF;
char modesave = 0x01;
char modeflag = 0x00;
// function prototype
int restore(void);
void main(void) {
EnableInterrupts; /* enable interrupts */
/* include your code here */
for(;
{
__RESET_WATCHDOG(); /* feeds the dog */
} /* loop forever */
/* please make sure that you never leave main */
}
/* function for Restore sounds in operation */
#pragma DATA_SEG DEFAULT
restore(void){
asm (
brclr 7,flag1,rstor1; //for the special case of interrupting !error C
18000
rts;
rstor1:
lda modesave; //find mode when interrupted
sta modeflag; //restore the flag
lda soundop;
and #$07f; //if these all off, nothing was operating
bne rstor2; //b/ something on, go figure it out
rts
;
rstor2:
return 0;
}
Hello Randall,
Seems you have to pretty much figure your inline assembly problems out for yourself, the compiler is not much help.
What about the TAX problem? It went away too? This was leading me to think the problem was something else.
I've never used inline assembly so don't know much about it. I can see you don't have a closing parenthesis for the asm( or maybe it's the stupid smilies. Use a code box inyour post to stop this happening.
Peg,
Thanks for the help, Umm code box, gotta figure that out on the forum.
I put the stupid smilies in there because I wanted to kill small woodland creatures when legit code did not run. (sorry). Talk to you Monday.
Regards
Randall
Try to use
__asm {
nop
}
(and not "asm(")
Also there must be a correspoding closing brace, of course.
The restore function should also have a return type, otherwise it defaults to int and the HLI code only returns a char.
Daniel
Hello Randall,
I can also see another issue with your function. You have used two intermediate RTS instructions. This is probably not a good idea when you need to return a value, since the actual value returned could be quite confusing if one of the RTS exits occurs.
Regards,
Mac
Hi,
Surely Codewarrior would issue a more relevant error than this for such simple things as " not in page zero" and " too big a relative branch" if these where the only problems???
There should be no limitation whatsoever on TAX
Hello,
The OP is a little unclear about the specifics of the error messages. However, since inline assembly code is used, I presume that the error messages are generated by the compiler, rather than the assembler. Therefore I guess the messages are likely to be more C orientated, and less specific for the assembly code content.
The error message that refers to opcode 45 (not sure whether hex or decimal) does not make sense. The opcode for TAX instruction is 0x97.
Regards,
Mac