Freescale 802.15.4 MAC???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale 802.15.4 MAC???

2,786 Views
admin
Specialist II

I have bassically two questions about the full (not the SMAC) Freescale 802.15.4 MAC:

 

1. Is there a way to know how many MAC retries has been used to transmit a message?

 

2. If a radio receive two times the same packet (in the case the  first ack was send but not receive by the transmitter), is the second packet discard by the MAC layer? If not, is there a way to have access to the sequence number of the received packet?

 

Thanks in advance for your help!

Fred

Labels (1)
0 Kudos
Reply
3 Replies

1,738 Views
xiaof
Contributor I
2. the second packet will be discard by the MAC layer,because those two packets have the same sequence number.
0 Kudos
Reply

1,738 Views
xiaof
Contributor I

 

1. retries times is  a MAC constant:aMaxFrameRetries,it's value is 3. 

0 Kudos
Reply

1,738 Views
admin
Specialist II
Anyone understanding these issues?
0 Kudos
Reply