ADC on MC9S08 : 8bits; Hight speed; single conversion

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC on MC9S08 : 8bits; Hight speed; single conversion

1,789 次查看
Iko
Contributor II

Hi all i'll try to do this way. Could you confirm that this work?

 

First, i made an init:

 

 

static void adc_init(void)   {#ifndef FAKEDEV   APCTL1 = 0x0F ;  // Desable buffers I/O  for pins:   APCTL2 = 0x8F ;  // ADP 0->3;8->11;15;16->19; et 21->23   APCTL3 = 0xEF ;  // Pin PORT A;B and C   ADCSC2 = 0x00 ;  //raz & config reg SC2 . Start convertion by write on ADCSC1;   ADCCV  = 0x00 ;   //No save of compared value   ADCCFG = 0x00 ;  //Full power (hight speed)                    //Clock divide by 1                    //Standard sampling time (3.5 adc clocks)                    //8 bits operations                    //Bus clk selected   ADCSC1 = 0x1F ;  //Clear Flag conversion Complet (COCO)                    //NO Interrupt                    //Single conversion Mode                    //ADC DISABLE => ADCH = 11111;#endif   }

 

 

during my program, i call a simple function with channel parameter "voie"

 

 

static U8 adc_lecture(U8 voie)   {   U8 value = 0 ; //U8 is define as unsigned char#ifndef FAKEDEV   ADCSC1 = voie ;   while (! ADCSC1_COCO)      {      ;      }   value = ADCRL;   ADCSC1 = 0x1F ;#endif   return value ;   }

 

 

Do you think it's a good way?

ty in advance...

标签 (1)
0 项奖励
回复
2 回复数

954 次查看
bigmac
Specialist III

Hello,

 

It is unclear to me why your functions might be "static".

 

While it will do no harm, the writing of the value 0x1F to ADCSC1 after each conversion is probably unnecessary since the ADC should automatically enter a lower power mode on completion of each conversion.

 

For your wait loop, the following code would suffice -

while (!ADCSC1_COCO);

 

 

Regards,

Mac

 

0 项奖励
回复

954 次查看
Iko
Contributor II

Hi big mac ^^

Ty for this answer.

 

I hadn't see that it go to low power after each conversion....

In addition, you write "should" (scuse i'm french ^^).

To be sure that it stop, i prefer write 0x1F to disable ADC...

 

TY ^^

0 项奖励
回复