9SO8QG8 CLOCK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

9SO8QG8 CLOCK

3,433 次查看
euge
Contributor I
hi
 
Í'm testing a 9S08QG8 by first time  with a 4MHz oscillator in FBE mode.
 
On Data sheet  and other freescale documents
fbus=(fext*1/BDIV)/2  = 1/tcyc    where tcyc is time machine cycle 
 
I used BDIV=1 ==> divide by 2
Then fbus=4MHz/4=1MHz ==> tcyc=1us      
 
I tryed to check this,  generating a square wave with
 
C code                                                                            Assembler code
 
for(;:smileywink:   {      PTBD_PTBD2=1;                                                     44:       PTBD_PTBD2=1;                                                                                       0014    1400    BSET  2,_PTBD          //2 cycles      _asm NOP                                                                45:       _asm NOP                                                                                       0016     9d       NOP                              //1 cycle      PTBD_PTBD2=0;                                                     46:       PTBD_PTBD2=0;                                                                                       0017    1500     BCLR  2,_PTBD          //2 cycles     _asm NOP                                                                 47:      _asm NOP                                                                                        0019    9d         NOP                            //1 cycle  
   __RESET_WATCHDOG(); // feeds the dog   } // loop forever 
 
If tcyc is  1 us I would have to obtain a 3 us period square wave but I obtain a 6 us period.
Maybe fext is fcrystal/2 and this information is not well documented or tcyc is not 1/fbus.
Maybe some of you with more experience have a response.
I regulary use 9S12,  GP32 and QT2 MCUs and I never had this discrepancy.
Best Regard 
标签 (1)
0 项奖励
回复
4 回复数

1,496 次查看
Ake
Contributor III
Hello,
I wrote your code and tested it,
 
void qc8intosc(void) {
SOPT1_COPE = 0;//turn off the watchdog
        PTBDD_PTBDD6 = 1;
 
 for(;:smileywink: {     //this loop takes 13 clock cycles to execute  
  PTBD_PTBD6 = 1;
  PTBD_PTBD6 = 0;
  } /* loop forever */
}
It will oscillate at 304 kHz.
As the loop takes 13 clocks to execute, this means that the fOP is 13 * 304 kHz = 3.95 MHz.
 
 I have not got an external oscillator, so I cannot test your conditions, but maybe this helps?
 
Regards,
Ake

 
0 项奖励
回复

1,496 次查看
euge
Contributor I
Ake, Bigmac Thank both for your time thinking about my doubts. The solution is that BSET or BCLR use 5 cycles not 2 cycles. I thought that each opcode and each operand corresponds to a cycle. That occurs when you do not consult the manual!!!!!!!! Best Regards
Eugenio
 
0 项奖励
回复

1,496 次查看
bigmac
Specialist III
Hello,
 
Further to the comments by Ake, the number of cycles required by BSET or BCLR instructions will be 5 cycles, and not 2 cycles.  Additionally, you did not allow for __RESET_WATCHDOG() macro, (assume 4 cycles), and for a BRA instruction to provide a continuous loop (3 cycles).  This would mean that your code should loop every 19 cycles, (assuming no interrupts).  Because of the additional overheads, the waveform will be asymmetric.
 
Regards,
Mac
 
0 项奖励
回复

1,496 次查看
euge
Contributor I
Ake, Bigmac

 


Thank both for your time thinking about my doubts.
The solution is that BSET or BCLR use 5 cycles not 2 cycles.
I thought that each opcode and each operand corresponds to a cycle.
That occurs when you do not consult the manual!!!!!!!!
Best Regards!!!!
0 项奖励
回复