802.15.4 PHY/MAC protocol stack for CodeWarrior V5.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

802.15.4 PHY/MAC protocol stack for CodeWarrior V5.0

2,106 Views
Vianney
Contributor I
Hello.

First of all, I don't know if "8-Bit Microcontrollers forum" is the right place to post this message, if not, I'm sorry.

So, I wonder if there is a version of the "802.15.4 PHY/MAC protocol stack" for CodeWarrior V5.0. Now I am working with CodeWarrior V5.0 but I have only the version of the "802.15.4 PHY/MAC protocol stack" for CodeWarrior V3.1.
I have to convert and port too the stack, I have tried to do that but the issue of this work is not so good. So if someone have a suggestion reguard to the different versions of this protocol stack, it will be great.

Vianney
Labels (1)
0 Kudos
Reply
1 Reply

1,144 Views
NLFSJ
Contributor III
Hi,
 

In answer to your question, if you are using the older MAC version, with 5.0 and it asks you to covert, just press cancel. The code will work fine.

You can upgrade to the latest version of the MAC that supports 5.0 by downloading the BeeKit. This is a GUI configuration program that contains the SMAC and MAC software.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT&...

Regards,

Nina

0 Kudos
Reply