32 bits Math Operations HCS08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

32 bits Math Operations HCS08

Jump to solution
2,510 Views
adrianodangelo
Contributor I

Hello All,

 

 

I am new on Codewarrior and in my current project(9S08PA8) I need a 32 bits variable to receive the result of a math operation.

This variable will receive a value from a single  multiply operation(eg. ADC_result x 87).

Below a snippet of my code:

 

 

uint8_t Mult=87;

uint32_t temp=0;

.

.

.

temp=(uint32_t)(adc_result0*Mult);

 

 

What happens is that if the value of adc_result0 is below or equal to 753 (the result ocupy only 2 bytes) everything is ok, but if the adc_result0 is higher than 753 (the result does not fill in 2 bytes) the compiler casts the result to 2 bytes. My question is can the HCS08 compiler operate in 32 bits variables? If not, what workaround can I use to solve this problem? (I tried to declare the variable as dword, unsigned long, long, without success).

 

Thanks,

Labels (1)
0 Kudos
Reply
1 Solution
2,300 Views
kef2
Senior Contributor V

This is how C works. 16 bits operation gives 16 bits result. You need to implicitly cast at least one of multipliers to 32 bits to get 32 bits product.

temp=(uint32_t)( (uint32_t)adc_result0*Mult);

Regards,

Edward

View solution in original post

0 Kudos
Reply
2 Replies
2,301 Views
kef2
Senior Contributor V

This is how C works. 16 bits operation gives 16 bits result. You need to implicitly cast at least one of multipliers to 32 bits to get 32 bits product.

temp=(uint32_t)( (uint32_t)adc_result0*Mult);

Regards,

Edward

0 Kudos
Reply
2,300 Views
adrianodangelo
Contributor I

Thank you Eduards,

Perfect! You solved my problem and saved me a lot of time.

0 Kudos
Reply