1321x: One Balun or Two?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1321x: One Balun or Two?

1,686件の閲覧回数
glowbrain
Contributor I
Has anyone doen a comparison between the one and two balun solutions shown in the freescale reference designs? It would be interesting to know the advantages and disadvantages.
I cant imagine going to the one balun solution for the sake of price alone (a few cents worth of components) if the performance were severly compromised.
On the other hand, if the performance is similar, why bother with the two balun solution?
ラベル(1)
0 件の賞賛
返信
1 返信

1,120件の閲覧回数
Alex_RUS
Contributor I
I tasted boards whith 2 baluns and boards with 1 balun. I did not meter dbms but I can say that boards with 2 baluns about 20% more effective.
0 件の賞賛
返信