08SH8 Crystal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

08SH8 Crystal

跳至解决方案
1,464 次查看
Juls
Contributor III

Hi

Im trying to setup my FOXS/040 crystal

a 4Mhz thu hole crystal

its connected to pin 5 and 6

with a 20pF to ground on each pin

 

Ive use device initialisation to set external clock source with 4 mhz

 

but the application always stop at the line waiting for crystal initialisation

at scope pin 5 is low and pin 6 is high

nothings is oscillating there :smileyfrustrated:

 

Any idea?

标签 (1)
0 项奖励
回复
1 解答
1,014 次查看
pgo
Senior Contributor V

Dear Juls,

 

Do you have the bias resistor (usually 10M)?

 

See section 2.2.2 Oscillator (XOSC) of the SH8  data sheet for oscillator component discussion.

 

bye

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,014 次查看
Juls
Contributor III

Thanks for pointing me that mistake

It was the problem

0 项奖励
回复
1,015 次查看
pgo
Senior Contributor V

Dear Juls,

 

Do you have the bias resistor (usually 10M)?

 

See section 2.2.2 Oscillator (XOSC) of the SH8  data sheet for oscillator component discussion.

 

bye

0 项奖励
回复