08SH8 Crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,363件の閲覧回数
Juls
Contributor III

Hi

Im trying to setup my FOXS/040 crystal

a 4Mhz thu hole crystal

its connected to pin 5 and 6

with a 20pF to ground on each pin

 

Ive use device initialisation to set external clock source with 4 mhz

 

but the application always stop at the line waiting for crystal initialisation

at scope pin 5 is low and pin 6 is high

nothings is oscillating there :smileyfrustrated:

 

Any idea?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,913件の閲覧回数
pgo
Senior Contributor V

Dear Juls,

 

Do you have the bias resistor (usually 10M)?

 

See section 2.2.2 Oscillator (XOSC) of the SH8  data sheet for oscillator component discussion.

 

bye

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,913件の閲覧回数
Juls
Contributor III

Thanks for pointing me that mistake

It was the problem

0 件の賞賛
返信
1,913件の閲覧回数
pgo
Senior Contributor V

Dear Juls,

 

Do you have the bias resistor (usually 10M)?

 

See section 2.2.2 Oscillator (XOSC) of the SH8  data sheet for oscillator component discussion.

 

bye

0 件の賞賛
返信