08SH8 Crystal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

08SH8 Crystal

Jump to solution
2,239 Views
Juls
Contributor III

Hi

Im trying to setup my FOXS/040 crystal

a 4Mhz thu hole crystal

its connected to pin 5 and 6

with a 20pF to ground on each pin

 

Ive use device initialisation to set external clock source with 4 mhz

 

but the application always stop at the line waiting for crystal initialisation

at scope pin 5 is low and pin 6 is high

nothings is oscillating there :smileyfrustrated:

 

Any idea?

Labels (1)
0 Kudos
Reply
1 Solution
1,789 Views
pgo
Senior Contributor V

Dear Juls,

 

Do you have the bias resistor (usually 10M)?

 

See section 2.2.2 Oscillator (XOSC) of the SH8  data sheet for oscillator component discussion.

 

bye

View solution in original post

0 Kudos
Reply
2 Replies
1,789 Views
Juls
Contributor III

Thanks for pointing me that mistake

It was the problem

0 Kudos
Reply
1,790 Views
pgo
Senior Contributor V

Dear Juls,

 

Do you have the bias resistor (usually 10M)?

 

See section 2.2.2 Oscillator (XOSC) of the SH8  data sheet for oscillator component discussion.

 

bye

0 Kudos
Reply