LPC5460x MCU Family Overview

Document created by Justin Mortimer Employee on Dec 19, 2016Last modified by Justin Mortimer Employee on Dec 19, 2016
Version 4Show Document
  • View in full screen mode

Getting Started with LPCXpresso54608 & MCUXpresso is pretty straight forward, but we want to make the process even easier.  So we created a simple guide to walk you through the getting started process,

      LPCXpresso54608: Out of Box & Getting Started Introduction

 

LPC5460x MCU Family part numbering & feature summary table (highlighted in yellow are the first of many parts to be released).

 

If it wasn't already clear, LPCXpresso54608 is the superset development board for our LPC5460x MCU Family.

Key features of the LPCXpresso54608 development board,

  • 272x480 color LCD with capacitive touch screen
  • On-board, high-speed USB, Link2 debug probe with CMSIS-DAP and SEGGER J-Link protocol options
  • UART and SPI port bridging from LPC546xx target to USB via the on-board debug probe
  • Support for external debug probe
  • 3 x user LEDs, plus Reset, ISP (3) and user buttons
  • Multiple Expansion options, including Arduino UNO and PMod
  • Built-in power consumption measurement for target LPC546xx MCU
  • 128Mb Micron MT25QL128 Quad-SPI flash
  • 8MB Micron MT48LC8M16A2B4 SDRAM
  • Knowles SPH0641LM4H digital microphone
  • Full size SD/MMC card slot
  • NXP MMA8652FCR1 accelerometer
  • Stereo audio codec with line in/out
  • High and full speed USB ports with micro A/B connector for host or device functionality
  • 10/100Mbps Ethernet (RJ45 connector)
16 people found this helpful

Attachments

    Outcomes