1. INTRODUCTION:
This document explains the general and basic steps to customize U-Boot for your own board. The board used in this document it is a working and stable board, the UDOO board (http://udoo.org).
2. REQUIREMENTS:
3. ADDING i.MX6 CUSTOM BOARD SUPPORT FOR U-BOOT.
This section follows the steps found in Chapter 1 of the i.MX6 BSP Porting Guide of the Yocto documentation (L3.14.28) https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&location=null&fpsp=1&WT_... .
$ cp -R board/freescale/mx6sabresd/ board/freescale/mx6_udoo
$ cp include/configs/mx6sabresd.h include/configs/mx6_udoo.h
Active arm armv7 mx6 freescale mx6_udoo mx6_udoo mx6_udoo:IMX_CONFIG=board/freescale/mx6_udoo/mx6dl_4x_mt41j128.cfg,MX6Q,DEFAULT_FDT_FILE="imx6q-udoo.dtb",DDR_MB=1024
obj-y := mx6sabresd.o
#!/bin/bash
export ARCH=arm
export CROSS_COMPILE=/opt/poky/1.7/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-
make distclean;
make mx6_udoo_config
make
$./build_u-boot.sh
4. CUSTOMIZING BOARD CODE
/*
* Device Configuration Data (DCD)
*
* Each entry must have the format:
* Addr-type Address Value
*
* where:
* Addr-type register length (1,2 or 4 bytes)
* Address absolute address of the register
* value value to be stored in the register
*/
DATA 4, 0x020e0774, 0x000C0000
DATA 4, 0x020e0754, 0x00000000
DATA 4, 0x020e04ac, 0x00000030
DATA 4, 0x020e04b0, 0x00000030
DATA 4, 0x020e0464, 0x00000030
DATA 4, 0x020e0490, 0x00000030
DATA 4, 0x020e074c, 0x00000030
DATA 4, 0x020e0494, 0x00000030
DATA 4, 0x020e04a0, 0x00000000
The .cfg files used in this example were taken from an old U-Boot version (2009) non dtb capable. The used files are found in the attached .zip file.
U-Boot calls already defined functions from a function pointer array that takes care of the board initialization at different stages. For example the board_early_init_f() is called at an early phase where we can disable the wdog and initialize the uart pins; board_init() and board_late_init() are called after board_early_init_f().
The WDOG pins need to be configured and in the mx6_udoo.c file a global struct configuration for those pins is declared, as well as macros for each pin
#define WDT_EN IMX_GPIO_NR(5, 4)
#define WDT_TRG IMX_GPIO_NR(3, 19)
iomux_v3_cfg_t const wdog_pads[] = {
MX6_PAD_EIM_A24__GPIO5_IO04 | MUX_PAD_CTRL(NO_PAD_CTRL),
MX6_PAD_EIM_D19__GPIO3_IO19,
};
static void setup_iomux_wdog(void)
{
imx_iomux_v3_setup_multiple_pads(wdog_pads, ARRAY_SIZE(wdog_pads));
gpio_direction_output(WDT_TRG, 0);
gpio_direction_output(WDT_EN, 1);
gpio_direction_input(WDT_TRG);
}
This configuration needs to be called at some point of the board_early_init_f()
int board_early_init_f(void)
{
setup_iomux_wdog();
This way the board_early_init_f() calls the iomux for the external wdog and disables it.
iomux_v3_cfg_t const uart2_pads[] = {
MX6_PAD_EIM_D26__UART2_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
MX6_PAD_EIM_D27__UART2_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),
};
This configuration should be called at early stage too.
static void setup_iomux_uart(void)
{
imx_iomux_v3_setup_multiple_pads(uart2_pads, ARRAY_SIZE(uart2_pads));
}
int board_early_init_f(void)
{
setup_iomux_wdog();
setup_iomux_uart();
Also the UART BASE register has to be defined as well as the console device. This is defined in the include/configs/mx6_udoo.h file.
#define CONFIG_MXC_UART_BASE UART2_BASE
#define CONFIG_CONSOLE_DEV "ttymxc1"
#define CONFIG_SYS_FSL_USDHC_NUM 3
#define CONFIG_SYS_MMC_ENV_DEV 0 /* SDHC3 */
The USDHC3 pin configuration has to be defined:
iomux_v3_cfg_t const usdhc3_pads[] = {
MX6_PAD_SD3_CLK__SD3_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_CMD__SD3_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT0__SD3_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT1__SD3_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT2__SD3_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_SD3_DAT3__SD3_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NANDF_D0__GPIO2_IO00 | MUX_PAD_CTRL(NO_PAD_CTRL), /* CD */
};
struct fsl_esdhc_cfg usdhc_cfg[1] = {
{USDHC3_BASE_ADDR, 0, 4},
};
This must be called and configured from the board_mmc_init() function:
int board_mmc_init(bd_t *bis)
{
s32 status = 0;
imx_iomux_v3_setup_multiple_pads(
usdhc3_pads, ARRAY_SIZE(usdhc3_pads));
usdhc_cfg[0].sdhc_clk = mxc_get_clock(MXC_ESDHC3_CLK);
status |= fsl_esdhc_initialize(bis, &usdhc_cfg[0]);
return status;
}
iomux_v3_cfg_t const enet_pads1[] = {
MX6_PAD_ENET_MDIO__ENET_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_MDC__ENET_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TXC__RGMII_TXC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD0__RGMII_TD0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD1__RGMII_TD1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD2__RGMII_TD2 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TD3__RGMII_TD3 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_TX_CTL__RGMII_TX_CTL | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_REF_CLK__ENET_TX_CLK | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RXC__RGMII_RXC | MUX_PAD_CTRL(ENET_PAD_CTRL),
/* RGMII reset */
MX6_PAD_EIM_D23__GPIO3_IO23 | MUX_PAD_CTRL(NO_PAD_CTRL),
/* alimentazione ethernet*/
MX6_PAD_EIM_EB3__GPIO2_IO31 | MUX_PAD_CTRL(NO_PAD_CTRL),
/* pin 32 - 1 - (MODE0) all */
MX6_PAD_RGMII_RD0__GPIO6_IO25 | MUX_PAD_CTRL(NO_PAD_CTRL),
/* pin 31 - 1 - (MODE1) all */
MX6_PAD_RGMII_RD1__GPIO6_IO27 | MUX_PAD_CTRL(NO_PAD_CTRL),
/* pin 28 - 1 - (MODE2) all */
MX6_PAD_RGMII_RD2__GPIO6_IO28 | MUX_PAD_CTRL(NO_PAD_CTRL),
/* pin 27 - 1 - (MODE3) all */
MX6_PAD_RGMII_RD3__GPIO6_IO29 | MUX_PAD_CTRL(NO_PAD_CTRL),
/* pin 33 - 1 - (CLK125_EN) 125Mhz clockout enabled */
MX6_PAD_RGMII_RX_CTL__GPIO6_IO24 | MUX_PAD_CTRL(NO_PAD_CTRL),
};
static iomux_v3_cfg_t const enet_pads2[] = {
MX6_PAD_RGMII_RD0__RGMII_RD0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RD1__RGMII_RD1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RD2__RGMII_RD2 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RD3__RGMII_RD3 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_RGMII_RX_CTL__RGMII_RX_CTL | MUX_PAD_CTRL(ENET_PAD_CTRL),
};
static void setup_iomux_enet(void)
{
imx_iomux_v3_setup_multiple_pads(enet_pads1, ARRAY_SIZE(enet_pads1));
udelay(20);
gpio_direction_output(IMX_GPIO_NR(2, 31), 1); /* Power on enet */
gpio_direction_output(IMX_GPIO_NR(3, 23), 0); /* assert PHY rst */
gpio_direction_output(IMX_GPIO_NR(6, 24), 1);
gpio_direction_output(IMX_GPIO_NR(6, 25), 1);
gpio_direction_output(IMX_GPIO_NR(6, 27), 1);
gpio_direction_output(IMX_GPIO_NR(6, 28), 1);
gpio_direction_output(IMX_GPIO_NR(6, 29), 1);
udelay(1000);
gpio_set_value(IMX_GPIO_NR(3, 23), 1); /* deassert PHY rst */
/* Need delay 100ms to exit from reset. */
udelay(1000 * 100);
gpio_free(IMX_GPIO_NR(6, 24));
gpio_free(IMX_GPIO_NR(6, 25));
gpio_free(IMX_GPIO_NR(6, 27));
gpio_free(IMX_GPIO_NR(6, 28));
gpio_free(IMX_GPIO_NR(6, 29));
imx_iomux_v3_setup_multiple_pads(enet_pads2, ARRAY_SIZE(enet_pads2));
}
Let's notice that the external PHY is not the same as the SABRESD AR8031. The UDOO features the MICREL KSZ9031 PHY. The latter needs to be defined and the former undefined in the include/configs/mx6_udoo.h file.
#undef CONFIG_PHY_ATHEROS
#define CONFIG_PHY_MICREL
#define CONFIG_PHY_MICREL_KSZ9031
Besides the PHY address has to be changed.
#define CONFIG_FEC_MXC_PHYADDR 6
The mx6_udoo.c file contains a setup_display function that configures the LDB module. This functions is called in the board_early_init_f(). With the current clock configuration is not possible to get the 33.2MHz for the LVDS and a different clock source for the LDB module must be chosen. The backlight and lvds power signals must be on.
The current configuration uses the mmdc_ch1 clock and to get closer to 33.26MHz the PLL2_PFD0 is chosen.
gpio_direction_output(IMX_GPIO_NR(1, 2), 1); /* LVDS power On */
gpio_direction_output(IMX_GPIO_NR(1, 4), 1); /* LVDS backlight On */
imx_iomux_v3_setup_multiple_pads(di0_pads, ARRAY_SIZE(di0_pads));
enable_ipu_clock();
imx_setup_hdmi();
/* Turn on4LDB0, LDB1, IPU,IPU DI0 clocks */
reg = readl(&mxc_ccm->CCGR3);
reg |= MXC_CCM_CCGR3_LDB_DI0_MASK | MXC_CCM_CCGR3_LDB_DI1_MASK;
writel(reg, &mxc_ccm->CCGR3);
/* set LDB0, LDB1 clk select to 011/011 */
reg = readl(&mxc_ccm->cs2cdr);
reg &= ~(MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_MASK
| MXC_CCM_CS2CDR_LDB_DI1_CLK_SEL_MASK);
reg |= (1 << MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_OFFSET)
| (1 << MXC_CCM_CS2CDR_LDB_DI1_CLK_SEL_OFFSET);
writel(reg, &mxc_ccm->cs2cdr);
With this changes you can compile the new U-Boot image with ./build_u-boot.sh and then just copy the uboot.imx file to your sd:
# sudo cp if=uboot.imx of=/dev/sdX bs=512 seek= 2 && sync
5. TESTING YOUR CHANGES
Inser the sd with the U-Boot image to micro sd slot and power up the board. You should get the U-Boot serial console like shown below.
In the console you can test the ethernet and phy configuration with the PING command:
I hope you find these basic steps useful for different boards.
Hi,
Thank you for this valuable information.
Does the iomux in kernel (from device tree) shall override the iomux in u-boot ?
Regards,
Ran
Can you give the solution for below screenshots
shanthu_1306_0-1721728068260.png