CW MCU v10.5 for 8bit MCU Banked Memory Patch Installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW MCU v10.5 for 8bit MCU Banked Memory Patch Installation

CW MCU v10.5 for 8bit MCU Banked Memory Patch Installation

User who work with CW MCU v10.5 for 8bit MCU that uses banked Memory(for example 9S08QE128, 9S08DZ128, etc), MUST install CW MCU v10.5 MCU Banked Memory Patch. Otherwise CW can NOT work with banked memory normally.

 

attached is the patch.

 

install instructions:

The CW MCU v10.5 Banked Memory Patch is for CodeWarrior Development Studio for Microcontrollers v10.5. It includes the files required to address the S08 banked memory defect in CW MCU v10.5. This patch is provided as a zip file with no automated installation scripts or programs. The zip file must be installed manually using the installation instructions below.

1. Close CW MCU v10.5.

2. Locate the CW MCU v10.5 installation on your hard drive. The default installation directory is: “C:\Freescale\CW MCU v10.5.”

3. Unzip “CW MCU v10.5 Banked Memory Patch.zip” into the MCU subdirectory (C:\Freescale\CW MCU v10.5\MCU). The files included in the zip file will overwrite the current files in the subdirectory.

-Or-

3. Use Windows Explorer to drag and drop the “bin” and “HC_Tools” subdirectories into the MCU subdirectory (C:\Freescale\CW MCU v10.5\MCU).

Labels (1)
Attachments
No ratings
Version history
Last update:
‎03-05-2014 04:04 AM
Updated by: