CW MCU v10.5 for 8bit MCU Banked Memory Patch Installation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW MCU v10.5 for 8bit MCU Banked Memory Patch Installation

CW MCU v10.5 for 8bit MCU Banked Memory Patch Installation

User who work with CW MCU v10.5 for 8bit MCU that uses banked Memory(for example 9S08QE128, 9S08DZ128, etc), MUST install CW MCU v10.5 MCU Banked Memory Patch. Otherwise CW can NOT work with banked memory normally.

 

attached is the patch.

 

install instructions:

The CW MCU v10.5 Banked Memory Patch is for CodeWarrior Development Studio for Microcontrollers v10.5. It includes the files required to address the S08 banked memory defect in CW MCU v10.5. This patch is provided as a zip file with no automated installation scripts or programs. The zip file must be installed manually using the installation instructions below.

1. Close CW MCU v10.5.

2. Locate the CW MCU v10.5 installation on your hard drive. The default installation directory is: “C:\Freescale\CW MCU v10.5.”

3. Unzip “CW MCU v10.5 Banked Memory Patch.zip” into the MCU subdirectory (C:\Freescale\CW MCU v10.5\MCU). The files included in the zip file will overwrite the current files in the subdirectory.

-Or-

3. Use Windows Explorer to drag and drop the “bin” and “HC_Tools” subdirectories into the MCU subdirectory (C:\Freescale\CW MCU v10.5\MCU).

标签 (1)
附件
无评分
版本历史
最后更新:
‎03-05-2014 04:04 AM
更新人: