CTU in MPC5744P (Model Based)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CTU in MPC5744P (Model Based)

Jump to solution
2,975 Views
haoxue1027
Contributor V

Hello.community

In my model,ADC1 can be triggered by CTU.

But,It is failed for ADC0.

Can you help solve the problem?

Thank you very much.

best regards

hao

0 Kudos
Reply
1 Solution
2,855 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

The model you've sent crushes all the Matlab versions I've tried to run it on. Maybe is because I am using the MBDT 3.2.0 and from the other thread I see that you are using the 3.1.0. Have you considered updating to our latest version?

Why don't you start from our example pwm_ctu_adc_mpc574xP.mdl?

Hope this helps,

Marius

View solution in original post

0 Kudos
Reply
3 Replies
2,855 Views
haoxue1027
Contributor V

mariuslucianandrei‌

Hello.

Sorry to trouble you,

Can you help me check the problem?

I have further confirmed the model.

The model I have built cannot work about ADC0 and ADC1 even though it is the same configuration as the demo"pwm_ctu_adc_mpc574xP".

But the demo can work normally on the board devkit-MPC5744P.

Is this a bug here?

My matlab version is 2019b.

Thank you very much.

best regards

hao

0 Kudos
Reply
2,856 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

The model you've sent crushes all the Matlab versions I've tried to run it on. Maybe is because I am using the MBDT 3.2.0 and from the other thread I see that you are using the 3.1.0. Have you considered updating to our latest version?

Why don't you start from our example pwm_ctu_adc_mpc574xP.mdl?

Hope this helps,

Marius

0 Kudos
Reply
2,855 Views
haoxue1027
Contributor V

Hello,Marius.

Thank you for replying.

I will update my version and check it again.

best regards

hao

0 Kudos
Reply