MPEG2TS File Parsing Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPEG2TS File Parsing Failed

4,780 Views
m_syed_ahmed
Contributor III

Hi,

We were working in IMX6Q-VAR_SOM board in Android Marshmallow OS. We have mpeg2ts file which contains channels with aac_latm audio codec. We were using Freescale library (lib_mpg2_parser_arm11_elinux.3.0.so) for parsing. We are getting below log. Can you help us solve the issue?

02-12 16:37:52.421  3405  3431 I FslInspector: TryMpegType TS SUCCESS
02-12 16:37:52.421  3405  3431 D FslExtractor: FslExtractor::FslExtractor mime=video/mp2ts
02-12 16:37:52.421  3405  3431 D FslExtractor: FslExtractor::Init BEGIN
02-12 16:37:52.421  3405  3431 D FslExtractor: GetLibraryName lib_mpg2_parser_arm11_elinux.3.0.so
02-12 16:37:52.436  3405  3431 D FslExtractor: load parser name lib_mpg2_parser_arm11_elinux.3.0.so
02-12 16:37:52.436  3405  3431 D FslExtractor: FslExtractor::CreateParserInterface success
02-12 16:37:52.436  3405  3431 I FslExtractor: Core parser BLN_MAD-MMLAYER_MPG2PARSER_04.05.05  build on Oct 24 2016 10:26:49
02-12 16:37:52.555  3405  3431 I OMXPlayer: Mpeg2CreateParser:parser created successfully
02-12 16:37:52.555  3405  3431 D FslExtractor: createParser2 flag=1c,err=0
02-12 16:37:52.555  3405  3431 I FslExtractor: mReadMode=0,mNumTracks=24
02-12 16:37:52.555  3405  3431 I FslExtractor: bSeekable 0
02-12 16:37:52.555  3405  3431 D FslExtractor: FslExtractor::ParseMediaFormat BEGIN
02-12 16:37:52.555  3405  3431 D FslExtractor: ParseVideo index=0,type=6,subtype=0
02-12 16:37:52.555  3405  3431 I FslExtractor: ParseVideo width=0,height=0,fps=0,rotate=0
02-12 16:37:52.555  3405  3431 I FslExtractor: add video track index=0,source index=0,mime=video/avc
02-12 16:37:52.555  3405  3431 D FslExtractor: ParseAudio index=1,type=6,subtype=2
02-12 16:37:52.555  3405  3431 I FslExtractor: audio track 1, lanuage: eng
02-12 16:37:52.555  3405  3431 I FslExtractor: ParseAudio channel=0,sampleRate=0,bitRate=0,bitPerSample=0,audioBlockAlign=0
02-12 16:37:52.556  3405  3431 I FslExtractor: add audio track index=1,sourceIndex=1,mime=audio/mp4a-latm
02-12 16:37:52.556  3405  3431 D FslExtractor: FslExtractor::Init ret=0
02-12 16:37:52.558  3405  3431 D FslExtractor: FslExtractor::getTrack index=0
02-12 16:37:52.558  3405  3431 E FslExtractor: getTrack source string cnt=1
02-12 16:37:52.558  3405  3431 D FslExtractor: start track 0
02-12 16:37:52.558  3405  3431 D FslExtractor: source start track 0
02-12 16:37:52.558  3405  3431 D FslExtractor: FslExtractor::getTrack index=1
02-12 16:37:52.558  3405  3431 E FslExtractor: getTrack source string cnt=1
02-12 16:37:52.558  3405  3431 D FslExtractor: start track 1
02-12 16:37:52.558  3405  3431 D FslExtractor: source start track 1
02-12 16:37:52.588  3405  3431 W VideoCapabilities: Unrecognized profile/level 32768/2 for video/mp4v-es
02-12 16:37:52.593  3405  3431 W VideoCapabilities: Unrecognized profile/level 0/0 for video/mpeg2
02-12 16:37:52.593  3405  3431 W VideoCapabilities: Unrecognized profile/level 0/2 for video/mpeg2
02-12 16:37:52.593  3405  3431 W VideoCapabilities: Unrecognized profile/level 0/3 for video/mpeg2
02-12 16:37:52.598  3405  3431 W VideoCapabilities: Unsupported mime video/x-pn-realvideo
02-12 16:37:52.600  3405  3431 W VideoCapabilities: Unsupported mime video/x-divx
02-12 16:37:52.602  3405  3431 W VideoCapabilities: Unsupported mime video/x-div4
02-12 16:37:52.604  3405  3431 W VideoCapabilities: Unsupported mime video/x-div3
02-12 16:37:52.606  3405  3431 W VideoCapabilities: Unsupported mime video/x-xvid
02-12 16:37:52.609  3405  3431 W VideoCapabilities: Unsupported mime video/x-j2c
02-12 16:37:52.611  3405  3431 W VideoCapabilities: Unsupported mime video/x-flash-video
02-12 16:37:52.615  3405  3431 W AudioCapabilities: Unsupported mime audio/eac3
02-12 16:37:52.638  3405  3431 I VideoCapabilities: Unsupported profile 4 for video/mp4v-es
02-12 16:37:52.663  3405  3434 I OMXClient: Using client-side OMX mux.
02-12 16:37:52.667  1125  1790 W linker  : /system/lib/lib_aac_dec_v2_arm12_elinux.so has text relocations. This is wasting memory and prevents security hardening. Ple.
02-12 16:37:52.669  1125  1815 E OMXNodeInstance: setParameter(2d:Freescale.std._decoder.aac.sw-based, ParamAudioAndroidAacPresentation(0x6f400003)) ERROR: Unsupported)
02-12 16:37:52.669  1125  1790 I OMXPlayer: AudioFilter SetParameter OMX_IndexParamAudioOutputConvert
02-12 16:37:52.670  1125  1546 I OMXPlayer: AudioFilter SetParameter OMX_IndexParamAudioSendFirstPortSettingChanged 0
02-12 16:37:52.674  1125  3435 I OMXPlayer: SetupDecoder AAC-Plus decoder Wrapper  build on Dec  7 2017 18:13:52
02-12 16:37:53.905  3405  3438 I OMXClient: Using client-side OMX mux.
02-12 16:37:53.913  3405  3437 I MediaCodec: [OMX.Freescale.std.video_decoder.avc.v3.hw-based] setting surface generation to 3486721
02-12 16:37:53.918  3405  3438 I ACodec  : Send reorder config(0) to VPU
02-12 16:37:53.919  1125  1125 W OMXNodeInstance: [2e:Freescale.std._decoder.avc.v3.hw-based] component does not support metadata mode; using fallback
02-12 16:37:53.920  3405  3438 E ACodec  : [OMX.Freescale.std.video_decoder.avc.v3.hw-based] storeMetaDataInBuffers failed w/ err -1010
02-12 16:37:53.921  1125  1815 E OMXNodeInstance: getConfig(2e:Freescale.std._decoder.avc.v3.hw-based, ConfigCommonOutputCrop(0x700000f)) ERROR: IncorrectStateTransiti)
02-12 16:37:53.922  1125  1790 E OMXNodeInstance: getConfig(2e:Freescale.std._decoder.avc.v3.hw-based, ConfigCommonScale(0x7000005)) ERROR: IncorrectStateTransition(0x)
02-12 16:37:53.929  3405  3438 D SurfaceUtils: set up nativeWindow 0x90942e08 for 0x0, color 0x13, rotation 0, usage 0x8002900
02-12 16:37:53.973  1125  1125 I imx6.gralloc: open gpu gralloc module!
02-12 16:37:54.313  1125  3439 I vpu-lib : Product Info: i.MX6Q/D/S
02-12 16:37:54.401  1125  3439 I vpu-lib : <gpu> alloc handle: 0xb3f0bd40, paddr: 0x30e00000, vaddr: 0xa8ac0000
02-12 16:37:54.418  1125  3439 I vpu-lib : <gpu> alloc handle: 0xb3f0bd60, paddr: 0x31600000, vaddr: 0xa8a2b000
02-12 16:37:54.419  1125  3439 I vpu-lib : bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0
02-12 16:37:54.447  3405  3438 D SurfaceUtils: set up nativeWindow 0x90942e08 for 1920x1088, color 0x13, rotation 0, usage 0x8002900
02-12 16:37:55.172  3405  3431 I JB      : FailureCounter > 200 - Reset the player
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal: Internal runtime error.
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal: java.lang.NullPointerException: Attempt to invoke virtual method 'boolean android.os.Handler.post(java.lang.Run1
reference
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:            at com.google.android.exoplayer.MediaCodecTrackRenderer.drainOutputBuffer(MediaCodecTrackRenderer.java:1111)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at com.google.android.exoplayer.MediaCodecTrackRenderer.doSomeWork(MediaCodecTrackRenderer.java:623)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at com.google.android.exoplayer.SampleSourceTrackRenderer.doSomeWork(SampleSourceTrackRenderer.java:128)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at com.google.android.exoplayer.ExoPlayerImplInternal.doSomeWork(ExoPlayerImplInternal.java:432)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at com.google.android.exoplayer.ExoPlayerImplInternal.handleMessage(ExoPlayerImplInternal.java:211)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at android.os.Handler.dispatchMessage(Handler.java:98)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at android.os.Looper.loop(Looper.java:148)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at android.os.HandlerThread.run(HandlerThread.java:61)
02-12 16:37:55.175  3405  3431 E ExoPlayerImplInternal:         at com.google.android.exoplayer.util.PriorityHandlerThread.run(PriorityHandlerThread.java:40)
02-12 16:37:55.177  3405  3425 I TunerSessionWorker: ExoPlayer Error: 1 1
02-12 16:37:55.177  3405  3433 W UsbTunerDataSource: No data update for 5000ms. returning -1.
02-12 16:37:55.180  3405  3430 I UsbTunerDataSource: Streaming stopped
02-12 16:37:55.240  3405  3433 I PlaySampleExtractor: EoS
02-12 16:37:55.250  1125  3439 I vpu-lib : <gpu> alloc handle: 0xb3f0bda0, paddr: 0x33200000, vaddr: 0xa67cc000
02-12 16:37:55.292  1125  1790 I vpu-lib : <gpu> free handle: 0xb3f0bd60, paddr: 0x31600000, vaddr: 0xa8a2b000
02-12 16:37:55.292  1125  1790 I vpu-lib : <gpu> free handle: 0xb3f0bd40, paddr: 0x30e00000, vaddr: 0xa8ac0000
02-12 16:37:55.292  1125  1790 I vpu-lib : <gpu> free handle: 0xb3f0bda0, paddr: 0x33200000, vaddr: 0xa67cc000
02-12 16:37:55.337  3405  3431 D FslExtractor: close track 0
02-12 16:37:55.337  3405  3431 D FslExtractor: close track 1
02-12 16:37:55.337  3405  3431 D FslExtractor: FslMediaSource::~FslMediaSource
02-12 16:37:55.337  3405  3431 D FslExtractor: FslMediaSource::~FslMediaSource
02-12 16:37:55.339  3405  3431 D FslExtractor: FslExtractor::~FslExtractor
02-12 16:37:56.247  3405  3425 I TunerSession: [Profiler] Video available in 9691 ms
02-12 16:37:57.944  3405  3425 I TunerSessionWorker: [Profiler] stopPlayback() takes 0 ms
02-12 16:37:58.724  3405  3425 I DvbManager: Frontend Parameters {{{ freq(570000000) inver(2) stand(DVBT) mod(QAM_AUTO) OFDM bandw(0) crateHP(9) crateLP(9) con(6) tmod}
02-12 16:37:59.202  3405  3425 I [  220.910283] cx231xx #0: DVB transfer mode is ISO.
DvbManager: Lock status : true

Labels (3)
0 Kudos
Reply
4 Replies

4,559 Views
igorpadykov
NXP Employee
NXP Employee

Hi Syed

in general mpeg-ts requires "Extended multimedia feature package", may be it

is missing. Details can be found in sect.6.1 Extended multimedia feature package.

Issue may be posted on variscite support, as this board is supported directly by its vendor.

Variscite Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,558 Views
dominic_selvara
Contributor I
We have Jellybean source and it is working fine on our board for the MPEG2TS Stream.
 
I think, JellyBean is using FSLParser C file for parsing the MPEG2TS located in external/fsl_imx-omx folder, but the Marshmallow is using the FSLExtractor  C file located in frameworks/av folder. FSLExtractor is not parsing the MPEG2TS data.

 

We want to know whether the FSLExtractor  supports the MPEG2TS parser or not.
0 Kudos
Reply

4,559 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dominic

suggest to proceed with Commercial Support and Engineering Services | NXP 

Reason:

-  this is third party board and software not officially supported by nxp,

- outdated Marshmallow release is not supported,

- software from "Extended Feature Packages" also requires special support.

Best regards
igor

0 Kudos
Reply

4,559 Views
dominic_selvara
Contributor I

Here is another note from our Team:

We were using FSL library for MPEG2TS Parsing. Same library are used in JellyBean and Marshmallow. Both JellyBean and Marshmallow have similar Component Register entries for this library. But in JellyBean, its parsing fine and entering into FSLParser C file located in external/fsl_imx-omx folder. In Marshmallow, its not parsing and entering into FSLExtractor  C file located in frameworks/av folder.

 

We want to know why FSLExtractor is not parsing the MPEG2TS stream.

 

We asked NXP regarding the same. We got a reply as

https://community.nxp.com/thread/524867#comment-1270311

 

Then we checked with Variscite regarding this issue, we got a reply to check with NXP again

0 Kudos
Reply