Hi Dave,
Thanks a lot for your updated information.
So, now, after you add the pull up on the /HOLD pin, and enable the QE bit, can you make all the function works on your side?
If you still have question about it, please kindly let me know.
About the app, we have some FlexSPI for nor flash, but it is use the primary, no secondary app note now. ABout the boot pin config, and use of flashloader, you can refer to the doc in flashloader for RT1020:
Flashloader_RT1020_1.0_GA\Flashloader_RT1020_1.0_GA\doc
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------