1RF_4Antenna Demo with S32R274 and TEF810X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1RF_4Antenna Demo with S32R274 and TEF810X

2,108 Views
sushant_sg
Contributor II

Hi,

I am trying to execute 1RF_4Antenna_Demo with TEF810X and S32R274 RRU Board.

I followed the reference manual given in Docs folder as well as the description file available with the example project.

I have seen that the example project has required header file for RFE setup. But the AppRfeInit() function in main_c1.c file is written only for MR3003. 

Is the same example project is compatible with TEF810X? 

   If yes, How to execute it?

   If no, can you provide other demo project for the same?

Thanks & Regards,

Sushant Gosavi.

0 Kudos
Reply
0 Replies