Hi All,
We are using i.MX6SX on our custom boards and we have configured enet2 in RGMII mode and using TI DP83822 phy. With below pinmux and device tree initialization we see issue with mdc clock. The phy is configured in 2.5 Mhz/10 Mbit mode we see TX and RX clk are 2.5 Mhz. The ti phy driver is enabled in the kernel.
The issue we see is on ENET2_MDC there is no clock on this line and it's always low. I doubt there is no data transmission happening on MDIO line because of mdc clock issue and mdio probed is failing to idenitify the phy.
kernel is nxp patched 4.9.11_1.0.0-ga.
on terminal it gives the below output.
ifconfig eth1 192.168.1.10
ifconfig: SIOCSIFFLAGS: No such device
there is no transmission on rx,tx lines.
&fec2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet2>;
phy-mode = "rgmii";
phy-reset-gpios = <&gpio2 8 GPIO_ACTIVE_LOW>;
phy-handle = <ðphy1>;
phy-supply = <®_vref_3v3>;
fsl,magic-packet;
status = "okay";
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy1: ethernet-phy@1 {
reg = <1>;
};
};
};
pinctrl_enet2: enet2grp-1 {
fsl,pins = <
MX6SX_PAD_ENET1_MDIO__ENET2_MDIO 0xa0b1 /* mdio */
MX6SX_PAD_ENET1_MDC__ENET2_MDC 0xa0b1 /* mdc */
MX6SX_PAD_RGMII2_TXC__ENET2_RGMII_TXC 0xa0b9
MX6SX_PAD_RGMII2_TD0__ENET2_TX_DATA_0 0xa0b1
MX6SX_PAD_RGMII2_TD1__ENET2_TX_DATA_1 0xa0b1
MX6SX_PAD_RGMII2_TD2__ENET2_TX_DATA_2 0xa0b1
MX6SX_PAD_RGMII2_TD3__ENET2_TX_DATA_3 0xa0b1
MX6SX_PAD_RGMII2_TX_CTL__ENET2_TX_EN 0xa0b1
MX6SX_PAD_RGMII2_RXC__ENET2_RX_CLK 0x3081
MX6SX_PAD_RGMII2_RD0__ENET2_RX_DATA_0 0x3081
MX6SX_PAD_RGMII2_RD1__ENET2_RX_DATA_1 0x3081
MX6SX_PAD_RGMII2_RD2__ENET2_RX_DATA_2 0x3081
MX6SX_PAD_RGMII2_RD3__ENET2_RX_DATA_3 0x3081
MX6SX_PAD_RGMII2_RX_CTL__ENET2_RX_EN 0x3081
MX6SX_PAD_ENET2_CRS__ENET2_CRS 0x3081 // CRS
MX6SX_PAD_ENET2_COL__ENET2_COL 0x3081 // CLO
MX6SX_PAD_ENET2_RX_CLK__GPIO2_IO_8 0x17059 // phy reset
MX6SX_PAD_ENET2_TX_CLK__GPIO2_IO_9 0x17059 // interupt
>;
any information on this would be very helpful. Thanks.