adv7180 driver for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adv7180 driver for imx6q

Jump to solution
7,499 Views
117876317
Contributor I

Hello everyone :

   We are debuging ADV7180 on our board with iMX6Q and I use the kernel linux3.0.5. Now I have some problems :

1.  Can't get right frame;

2. /mxc_v4l2_tvin.out -iw 720 -ih 480 -ow 720 -oh 480

    

TV decoder chip is adv7180_decoder                                           
VIDIOC_G_FMT failed                                                          
driver=mxc_vout, card=DISP3 FG, bus=, version=0x00000000, capabilities=0x0402
fmt RGB565: fourcc = 0x50424752                                              
fmt BGR24: fourcc = 0x33524742                                               
fmt RGB24: fourcc = 0x33424752                                               
fmt RGB32: fourcc = 0x34424752                                               
fmt BGR32: fourcc = 0x34524742                                               
fmt NV12: fourcc = 0x3231564e                                                
fmt UYVY: fourcc = 0x59565955                                                
fmt YUYV: fourcc = 0x56595559                                                
fmt YUV422 planar: fourcc = 0x50323234                                       
fmt YUV444: fourcc = 0x34343459                                              
fmt YUV420: fourcc = 0x32315559                                              
fmt YVU420: fourcc = 0x32315659                                              
fmt TILED NV12P: fourcc = 0x50564e54                                         
fmt TILED NV12F: fourcc = 0x46564e54                                         
fmt YUV444 planar: fourcc = 0x50343434                                       
start time = 43 s, 122205 us  

 

    Now, I can't find why it does't work. Anyone help me. Thank you.

Original Attachment has been moved to: 问题描述.zip

Labels (2)
0 Kudos
Reply
1 Solution
6,858 Views
igorpadykov
NXP Employee
NXP Employee

Hi

it can be debugged using baremetal SDK (../camera/test/adv7180_capture.c),

please refer to sect.18.5.2.3 BT656 mode attached document

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
6,859 Views
igorpadykov
NXP Employee
NXP Employee

Hi

it can be debugged using baremetal SDK (../camera/test/adv7180_capture.c),

please refer to sect.18.5.2.3 BT656 mode attached document

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply