Hello everyone :
We are debuging ADV7180 on our board with iMX6Q and I use the kernel linux3.0.5. Now I have some problems :
1. Can't get right frame;
2. /mxc_v4l2_tvin.out -iw 720 -ih 480 -ow 720 -oh 480
TV decoder chip is adv7180_decoder
VIDIOC_G_FMT failed
driver=mxc_vout, card=DISP3 FG, bus=, version=0x00000000, capabilities=0x0402
fmt RGB565: fourcc = 0x50424752
fmt BGR24: fourcc = 0x33524742
fmt RGB24: fourcc = 0x33424752
fmt RGB32: fourcc = 0x34424752
fmt BGR32: fourcc = 0x34524742
fmt NV12: fourcc = 0x3231564e
fmt UYVY: fourcc = 0x59565955
fmt YUYV: fourcc = 0x56595559
fmt YUV422 planar: fourcc = 0x50323234
fmt YUV444: fourcc = 0x34343459
fmt YUV420: fourcc = 0x32315559
fmt YVU420: fourcc = 0x32315659
fmt TILED NV12P: fourcc = 0x50564e54
fmt TILED NV12F: fourcc = 0x46564e54
fmt YUV444 planar: fourcc = 0x50343434
start time = 43 s, 122205 us
Now, I can't find why it does't work. Anyone help me. Thank you.
Original Attachment has been moved to: 问题描述.zip
Solved! Go to Solution.
Hi
it can be debugged using baremetal SDK (../camera/test/adv7180_capture.c),
please refer to sect.18.5.2.3 BT656 mode attached document
Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
it can be debugged using baremetal SDK (../camera/test/adv7180_capture.c),
please refer to sect.18.5.2.3 BT656 mode attached document
Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------