How to reconfigure the NHS3100 startup state to take temperature measurements only under NFC field in battery-less application?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reconfigure the NHS3100 startup state to take temperature measurements only under NFC field in battery-less application?

Jump to solution
2,504 Views
stevewald
Contributor III

We need to reconfigure the NHS3100 startup state to take temperature measurements only under NFC field for a battery-less application. I don't see where in the TLogger sources that the initial state is configured. Can someone provide some hints or clues?

1 Solution
2,251 Views
driesmoors
NXP Employee
NXP Employee

The current firmware (SDK 10.1) will already make a temperature measurement each time is tapped by the phone, regardless whether it is configured or not. This value is also passed along in the NFC shared memory as a text record. You can have a look at that when you use the phone without any APP being active.

Have a look at

  • Init, file maintlogger.c, where TMeas_Measure is called.
  • ResponseCb, file msghandler.c, where NDEFT2T_CreateTextRecord is called.

View solution in original post

0 Kudos
Reply
3 Replies
2,252 Views
driesmoors
NXP Employee
NXP Employee

The current firmware (SDK 10.1) will already make a temperature measurement each time is tapped by the phone, regardless whether it is configured or not. This value is also passed along in the NFC shared memory as a text record. You can have a look at that when you use the phone without any APP being active.

Have a look at

  • Init, file maintlogger.c, where TMeas_Measure is called.
  • ResponseCb, file msghandler.c, where NDEFT2T_CreateTextRecord is called.
0 Kudos
Reply
2,251 Views
stevewald
Contributor III

Dries Moors had earned a badge for giving us more than this answer, including some source code to run a cleaner no-battery use case on the NHS3100. There are subtle problems with the initialization without a battery to maintain state. Thanks!

2,251 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

It is only required to flash the NHS3100 with TLogger example. You will be able to take temperature measurements every time you approach your phone to the device. This is accomplished because of the phone's field power provided to the device even if NHS3100 is no longer battery powered.

 

Regards,

Ivan.

0 Kudos
Reply