FT5X06 can't work properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FT5X06 can't work properly

3,666 Views
pengxingwei
Contributor III

Hi,

      My OS is Android_M6.0 and my board is imx6q sabresd,which kernel is linux 4.1.15,I want to point the ft5x06 touchscreen on it,now the driver is https://github.com/boundarydevices/linux-imx6/blob/boundary-imx-m6.0.1_1.0.0-ga/drivers/input/touchs...

my dts file is imx6qdl-sabresd.dtsi,

   

ft5x06_ts@38 {
compatible = "ft5x06,ft5x06-touch";
reg = <0x38>;

interrupts-extended = <&gpio6 2 IRQ_TYPE_EDGE_FALLING>;

reset-gpios = <<&gpio6 3 1>

wakeup-gpios = <&gpio6 2 GPIO_ACTIVE_LOW>;
};

now the system startup log :

now the touchscreen has respond ,but the touch point is not accuracy,the effect is as the picture

how to solve the problem .thanks

Labels (2)
0 Kudos
Reply
5 Replies

2,496 Views
igorpadykov
NXP Employee
NXP Employee

Hi peng

please try calibration as described on

How to use tslib calibration at i2c touch ft5x06 in Android 5.0  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,496 Views
pengxingwei
Contributor III

Hi ,I print the touch point :

Its value is  abnormal,why happen to it ?? What matters most is the circle didn't move with my finger. Thanks

0 Kudos
Reply

2,496 Views
igorpadykov
NXP Employee
NXP Employee

if you correctly calibrated it, its value should not be abnormal.

0 Kudos
Reply

2,496 Views
pengxingwei
Contributor III

Hi,igorpadykov:

            I install the calibration app failed,the app can't install on my device.

0 Kudos
Reply

2,496 Views
pengxingwei
Contributor III

Hi,thanks for your reply,

for my board the resolution is correct (1280 *800).but when i leave the screen and move to  other position ,sometimes the circle didn't move with my finger.the link:

How to use tslib calibration at i2c touch ft5x06 in Android 5.0  it can't solve my problem ,Are there others solution for it ?thanks!

0 Kudos
Reply