FT5X06 can't work properly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FT5X06 can't work properly

4,358 次查看
pengxingwei
Contributor III

Hi,

      My OS is Android_M6.0 and my board is imx6q sabresd,which kernel is linux 4.1.15,I want to point the ft5x06 touchscreen on it,now the driver is https://github.com/boundarydevices/linux-imx6/blob/boundary-imx-m6.0.1_1.0.0-ga/drivers/input/touchs...

my dts file is imx6qdl-sabresd.dtsi,

   

ft5x06_ts@38 {
compatible = "ft5x06,ft5x06-touch";
reg = <0x38>;

interrupts-extended = <&gpio6 2 IRQ_TYPE_EDGE_FALLING>;

reset-gpios = <<&gpio6 3 1>

wakeup-gpios = <&gpio6 2 GPIO_ACTIVE_LOW>;
};

now the system startup log :

now the touchscreen has respond ,but the touch point is not accuracy,the effect is as the picture

how to solve the problem .thanks

标签 (2)
0 项奖励
回复
5 回复数

3,188 次查看
igorpadykov
NXP Employee
NXP Employee

Hi peng

please try calibration as described on

How to use tslib calibration at i2c touch ft5x06 in Android 5.0  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,188 次查看
pengxingwei
Contributor III

Hi ,I print the touch point :

Its value is  abnormal,why happen to it ?? What matters most is the circle didn't move with my finger. Thanks

0 项奖励
回复

3,188 次查看
igorpadykov
NXP Employee
NXP Employee

if you correctly calibrated it, its value should not be abnormal.

0 项奖励
回复

3,188 次查看
pengxingwei
Contributor III

Hi,igorpadykov:

            I install the calibration app failed,the app can't install on my device.

0 项奖励
回复

3,188 次查看
pengxingwei
Contributor III

Hi,thanks for your reply,

for my board the resolution is correct (1280 *800).but when i leave the screen and move to  other position ,sometimes the circle didn't move with my finger.the link:

How to use tslib calibration at i2c touch ft5x06 in Android 5.0  it can't solve my problem ,Are there others solution for it ?thanks!

0 项奖励
回复