NIST statistical test failure on RNG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NIST statistical test failure on RNG

4,167 Views
dhanushkadangam
Contributor III

We are using the imx6ul processor in an application where we need to obtain certification for random number generation sources. For this, we capture ~128MB of random data from /dev/random, /dev/urandom and /dev/hwrng interfaces and feed it to NIST statistical tests. 

According to the Final Analysis Reports, "Overlapping (Periodic) Template Matching Test" scores below the minimum pass rate in all the above interfaces.

  • Why does this particular test fail on all interfaces?
  • What are the implications of this result on the certification?
  • Will some post-processing such as whitening help fix this?
  • Is there any specific configuration for the CAAM RNG that we should use? We are using yocto linux-3.14.38 without any modifications.

PS:

imx6ul SRM says the RNG should be instantiated in test mode to obtain data for certification. Even in test mode the above test fails. Below are extracts from the test reports for /dev/hwrng:

In normal mode:

------------------------------------------------------------------------------
 C1  C2  C3  C4  C5  C6  C7  C8  C9 C10  P-VALUE  PROPORTION  STATISTICAL TEST
------------------------------------------------------------------------------
  6   2   1   0   0   1   0   0   0   0  0.000199      6/10   *  OverlappingTemplate

In test mode:

------------------------------------------------------------------------------
 C1  C2  C3  C4  C5  C6  C7  C8  C9 C10  P-VALUE  PROPORTION  STATISTICAL TEST
------------------------------------------------------------------------------
  7   1   1   1   0   0   0   0   0   0  0.000003 *    5/10   *  OverlappingTemplate

The minimum pass rate for this test is 8 for a sample size of 10 binary sequences.

Labels (3)
2 Replies

3,411 Views
dhanushkadangam
Contributor III

It turned out that we had used wrong parameters for the test;

./assess 134217728

:

How many bitstreams? 10

when they should have been

./assess 1000000

:

How many bitstreams? 1073

With these new parameters, the Overlapping (Periodic) Template Matching Test passes for all interfaces.

0 Kudos
Reply

3,411 Views
igorpadykov
NXP Employee
NXP Employee

Hi dhanushka

RNG inside CAAM module i.MX6 is identical to the HW used
in NPD QorIQ devices based on NIST SP800-90.  NPD has obtained a certificate for
RNG and because the HW is the same this certificate also covers i.MX6 as well.    See

http://csrc.nist.gov/groups/STM/cavp/documents/drbg/drbgval.html Validation No 94.

Help with sertification tests can be obtained from Professional Services :

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply