Dear Joan joanxie
Thank you for replying.
I think vpu is typo of gpu which support multi-layer overlay.
BTW I found actual rate as following.
https://community.nxp.com/message/452579
DDR3-1066 32-bit reaches a maximum of ~2.5 GB/s in total (theoretic 4.2 GB/s)
DDR3-1066 64-bit reaches a maximum of ~2.8 GB/s in total (theoretic 8.5? GB/s)
My expectation is improved 40% (~4.0 GB/s in total) to use PRE in i.MX6QP.
If it true, fullHD-dual display(2x1920x1080x60/s=250MP/s) may possible for only 2 layer overlay implementation.
250MP/s x2 x4B/Pix =2GB/s //half of 4GB/s
I think it' not bad. How do you think?