NEW S32K-148 EVB Lab is on the web:
Hello
I have completed the hands-on lab for the S32K148 EVB and updated the lab for the S32K-144 EVB.
The S32K-148 EVB lab has detailed instructions on getting the ETM trace working along with Code Coverage and Performance Analysis.
Keil will soon release in November the new ULINKplus: this adds power measurement and other features. You can tie the current draw to your source code. www.keil.com/ulinkplus.
The S32K-148 EVB appnote is located here:
www.keil.com/appnotes/docs/apnt_305.asp
The updated lab for the S32K-144 EVB is located here:
www.keil.com/appnotes/docs/apnt_299.asp
Both of these include a very nice DSP example and a Blinky example.
I also have a lab for the popular NXP Cookbook.
www.keil.com/appnotes/docs/apnt_304.asp
A Keil ULINKpro is needed for ETM trace.
Keil MDK is free for up to 32K code size. All examples compile and run inside this limit.
It works with OpoenSDA or a selection of external debug adapters including any Keil ULINK or a J-Link.
Thanks
Bob Boys
San Jose, CA
[email protected]