Keil Hands-On Lab available for S32k-144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keil Hands-On Lab available for S32k-144

1,219 Views
robertboys
Contributor IV

Hello

This lab using Keil MDK is now available:  www.keil.com/appnotes/docs/apnt_299.asp

This shows the various debug facilities one can use with the S32K-144.

When I receive a S32K-148 board, I will add ETM Instruction Trace to this lab.

If you want to see what ETM can do:  look at the TWR-K64 lab: www.keil.com/appnotes/docs/apnt_288.asp

The ARM/Keil Software Pack is available now: www.keil.com/dd2/pack

This Pack is a regular .zip file with the extension changed to .pack.

It contains header files, examples and much more.

Thanks

Bob Boys

ARM

Tags (1)
1 Reply

821 Views
robertboys
Contributor IV

NEW  S32K-148 EVB Lab is on the web:

Hello

I have completed the hands-on lab for the S32K148 EVB and updated the lab for the S32K-144 EVB.

The S32K-148 EVB lab has detailed instructions on getting the ETM trace working along with Code Coverage and Performance Analysis.

Keil will soon release in November the new ULINKplus:  this adds power measurement and other features.  You can tie the current draw to your source code.  www.keil.com/ulinkplus.

The S32K-148 EVB appnote is located here:

 www.keil.com/appnotes/docs/apnt_305.asp

 

The updated lab for the S32K-144 EVB is located here:

 www.keil.com/appnotes/docs/apnt_299.asp

 

Both of these include a very nice DSP example and a Blinky example.

 

I also have a lab for the popular NXP Cookbook.

www.keil.com/appnotes/docs/apnt_304.asp 

A Keil ULINKpro is needed for ETM trace.

Keil MDK is free for up to 32K code size.  All examples compile and run inside this limit.

It works with OpoenSDA or a selection of external debug adapters including any Keil ULINK or a J-Link.

Thanks

Bob Boys

San Jose, CA

bob.boys@arm.com

0 Kudos