BT1120 1080P connect to imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BT1120 1080P connect to imx6q

3,149件の閲覧回数
jiejia
Contributor III

Hi,

  I'm using an i.mx6q-sabresd with a kernel based on linux3.0.35.

  There is a BT1120 1080P HD-SDI camera connected on CSI0 according to gv7601. the GV7601 does not need to be configured using SPI on our setup.  There are pulse output from gv7601, and the frequence of pclk is 74.25MHz. 

  I've manually applied the BT1120 patch to enable 16bit and 1120 from Support BT1120 progressive mode in Mx6Q 

  On the software side, I have that pinmuxing:

MX6Q_PAD_EIM_D27__IPU1_CSI0_D_0,
MX6Q_PAD_EIM_D26__IPU1_CSI0_D_1,
MX6Q_PAD_EIM_D31__IPU1_CSI0_D_2,
MX6Q_PAD_EIM_D30__IPU1_CSI0_D_3,
MX6Q_PAD_CSI0_DAT4__IPU1_CSI0_D_4,
MX6Q_PAD_CSI0_DAT5__IPU1_CSI0_D_5,
MX6Q_PAD_CSI0_DAT6__IPU1_CSI0_D_6,
MX6Q_PAD_CSI0_DAT7__IPU1_CSI0_D_7,
MX6Q_PAD_CSI0_DAT8__IPU1_CSI0_D_8,
MX6Q_PAD_CSI0_DAT9__IPU1_CSI0_D_9,
MX6Q_PAD_CSI0_DAT10__IPU1_CSI0_D_10,
MX6Q_PAD_CSI0_DAT11__IPU1_CSI0_D_11,
MX6Q_PAD_CSI0_DAT12__IPU1_CSI0_D_12,
MX6Q_PAD_CSI0_DAT13__IPU1_CSI0_D_13,
MX6Q_PAD_CSI0_DAT14__IPU1_CSI0_D_14,
MX6Q_PAD_CSI0_DAT15__IPU1_CSI0_D_15,
MX6Q_PAD_CSI0_DAT16__IPU1_CSI0_D_16,
MX6Q_PAD_CSI0_DAT17__IPU1_CSI0_D_17,
MX6Q_PAD_CSI0_DAT18__IPU1_CSI0_D_18,
MX6Q_PAD_CSI0_DAT19__IPU1_CSI0_D_19,

 

That is what I have in my data_capture[] :

        {
                .ipu = 0,
                .csi = 0,
                .mclk_source = 0,
                .is_mipi = 0,
        },

 

I also set CSI0 to parallel with:

    mxc_iomux_set_gpr_register(1, 19, 1, 1);

 

I tweaked drivers/media/video/mxc/capture/mxc_v4l2_capture.c to be able to set BT.1120 clock mode:

       csi_param.clk_mode = IPU_CSI_CLK_MODE_CCIR1120_PROGRESSIVE_SDR;
       csi_param.pixclk_pol = 0;
       csi_param.data_width = IPU_CSI_DATA_WIDTH_8;
       csi_param.mclk = 74250000;
       csi_param.Hsync_pol = 0;
       csi_param.Vsync_pol = 0;
       csi_param.ext_vsync = 0;

 

I end up with those register set (by drivers/mxc/ipu3/ipu_capture.c):

CSI_SENS_CONF = 0x82000950

CSI_SENS_FRM_SIZE = 0x0437077F

CSI_ACT_FRM_SIZE = 0x0437077F

CSI_OUT_FRM_CTRL = 0x0

exec this commond on console,  ./mxc_v4l2_capture.out  -iw 1920 -ih 1080 -ow 1280 -oh 800 -f YUYV -fr 25

in_width = 1920, in_height = 1080
out_width = 1280, out_height = 800
top = 0, left = 0

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
VIDIOC_DQBUF failed.
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
VIDIOC_QBUF failed

What am I missing ?  Any help will appreciated

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,979件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for hardware, pls check if you connect correctly refer to the path.

 for software,  you should set CSI0_SENS_DATA_FORMAT is 010 YUV422 (UYVY...)

https://community.nxp.com/thread/329485 

hope this link is helpful for you.

0 件の賞賛
返信

1,979件の閲覧回数
jiejia
Contributor III

Hi, Xie

  You are right. There are something wrong with my hardware. 

  

  Now it works:    ./mxc_v4l2_overlay.out -iw 1920 -ih 1080 -it 0 -il 0 -ow 1280 -oh 800 -ot 0 -ol 0 -fr 30

  But there are something with encoded:./mxc_v4l2_capture.out  -iw 1920 -ih 1080 -ow 1920 -oh 1080 -fr 30 test.yuv

in_width = 1920, in_height = 1080
out_width = 1920, out_height = 1080
top = 0, left = 0
sensor frame format: YUYV
g_fmt_cap returns widthxheight of input as 1920 x 1080
Width = 1920 Height = 1080 Image size = 3110400
pixelformat = 842093913
YUV420
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00100000

 when I decode test.yuv, it's abnormal.

0 件の賞賛
返信