How to read usb serial of k70 tower board using putty on ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to read usb serial of k70 tower board using putty on ubuntu

1,099 Views
sameerarvikar
Contributor III

I can read usb serial (i have put uboot on the kit)on in windows but when I connect it to ubuntu I cannot see ttyusb0 ,the kit is detected as I can see using dmesg

The kit is twr-k70F12.0M

Tags (1)
0 Kudos
Reply
1 Reply

984 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi sameer arvikar

In Ubuntu OS, CDC devices are recognized as ACM components. ACM described how devices conforming to the Communications devices class (CDC) should present themselves to the USB host. I connect the same board and you can see in the following image how it is listed.

pastedImage_2.png

Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply