How to read usb serial of k70 tower board using putty on ubuntu

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to read usb serial of k70 tower board using putty on ubuntu

1,036 次查看
sameerarvikar
Contributor III

I can read usb serial (i have put uboot on the kit)on in windows but when I connect it to ubuntu I cannot see ttyusb0 ,the kit is detected as I can see using dmesg

The kit is twr-k70F12.0M

标记 (1)
0 项奖励
回复
1 回复

921 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi sameer arvikar

In Ubuntu OS, CDC devices are recognized as ACM components. ACM described how devices conforming to the Communications devices class (CDC) should present themselves to the USB host. I connect the same board and you can see in the following image how it is listed.

pastedImage_2.png

Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复