"CM4 is in lockup" - when does it happen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"CM4 is in lockup" - when does it happen

Jump to solution
3,821 Views
dry
Senior Contributor I

There is a reset or interrupt source called "CM4 is in lockup". But what I cannot find in the Vybrid manual describing when can this happen.

When and why can this happen?

0 Kudos
Reply
1 Solution
3,305 Views
dry
Senior Contributor I

Hi Yuri,

ARM M4 manual says "..The processor enters a lockup state if a fault occurs when executing the NMI or HardFault handlers. "

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0553a/BGBFCHGC.html 

Thus it shouldn't be in the state just after system reset.

View solution in original post

1 Reply
3,306 Views
dry
Senior Contributor I

Hi Yuri,

ARM M4 manual says "..The processor enters a lockup state if a fault occurs when executing the NMI or HardFault handlers. "

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0553a/BGBFCHGC.html 

Thus it shouldn't be in the state just after system reset.