What is the min and max ODR accuracy on the MMA8451

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the min and max ODR accuracy on the MMA8451

2,209 Views
johncampbell
Contributor II

The typical ODR accuracy is stated in Table 2 of the datasheet as +- 2%. This is at 25 C.

There are no minimum or maximum values in the datasheet.

What tolerance over temperature could be expected?

regards johnc

0 Kudos
2 Replies

1,854 Views
johncampbell
Contributor II

Thanks for your prompt response. Answers my question.

regards johnc

0 Kudos

1,854 Views
reyes
NXP TechSupport
NXP TechSupport

Dear johnc,

This is actually not a typical value, this could be seen like: MIN = -2% and MAX = +2%

The total accuracy variations should not change more than this +/-2%

Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos