Will CSI MIPI need external vsync signal?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will CSI MIPI need external vsync signal?

3,640 Views
ifzhao
Contributor I

Dear all,

Now I'm working with a mipi camera on imx6 dual lite, after check the RM, I find :

YJ9]ME{VGZ(6JXX4OOMSBO0.jpg

However, I check through the RM file, and find one vsync pin for CSI0 parallel port but no vsync pin for CSI MIPI.

I  wonder if vsync is necessary to make MIPI working ?

Labels (3)
Tags (3)
0 Kudos
Reply
1 Reply

2,856 Views
igorpadykov
NXP Employee
NXP Employee

Hi If

external vsync signal is not needed, as synchs are embedded in mipi

stream, please check  Table 19-2. CSI2IPU output signals to IPU   vsync,hsync

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------