BSDL file for MK10DN512VMD10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSDL file for MK10DN512VMD10

2,965 Views
ockertvanschalk
Contributor II

Hi

I need the BSDL files for MK10DN512VMD10 (144-ball BGA) and MK10DN512VLQ10 (144-pin QFP). The archive listed under the device's Software & Tools page ("K10_100MHZ_BSDL (REV 0)", Download URL: http://cache.nxp.com/files/microcontrollers/hardware_tools/models/bsdl/K10_100MHZ_BSDL.zip ) only contains the BSDL file for the 121-pin version.

Thanks, regards

Ockie

5 Replies

2,622 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Ockert.

These files are requested on page Kinetis CAD Schematics, Symbols & Footprints|NXP

but currently there is an error on our side, I have reproduced the problem, I will let you know as soon as possible.

Thank you for your patience,

Best Regards,

Iva

0 Kudos
Reply

2,622 Views
ockertvanschalk
Contributor II

Hi Iva

Thank you for the response, I look forward to hearing from you.

Regards

Ockie

0 Kudos
Reply

2,621 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Ockie

Please check the attached file.

I hope this will help you

2,621 Views
ockertvanschalk
Contributor II

Hi Pedro

Thank you for supplying the BSDL file. However, it does not seem to have a valid IDCODE for my specific device, MK10DN512VMD10 (we are using both the 144MAPBGA and 144LQFP variants).

I am using the XJTAG XJLink device to connect to the processor, which reports the following:

____________________________________________________

Starting Check Chain...

1 Devices found

ID Codes read:

0x4BA00477

Chain intact - No errors found

IR length of chain: 4

Device 1 (No BSDL File)

Read : 01001011101000000000010001110111 (0x4BA00477)

____________________________________________________

If I now supply your BSDL file (K10_144BGA_13x13.bsdl) to the software, I get the following error:

XJLink Error.png

Can you explain why the device reports a different ID Code from that specified in the BSDL file?

Thanks, regards

0 Kudos
Reply

2,621 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Please give me some time to get the update file

Regards

Vicente Gomez

0 Kudos
Reply