playing video on i.mx6 two screens lagging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

playing video on i.mx6 two screens lagging

1,298 Views
andreykononov
Contributor III

i'm connect HDMI and LVDS screens to SABRE for Automotive and trying to play video file (1280x720) via qmlvideofx from QT examples on ech screen and it lagging a bit

kernel init cmd  (yocto jethro kernel )

bootargs console=${console},${baudrate} ${smp} root=${mmcroot} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:dev=ldb,1280x480M,if=RGB666,ldb=sin1

start scripts

root@imx6qsabreauto:~# cat /home/root/bin/hdmi.sh    

#!/bin/sh    

export QT_QPA_EGLFS_FB=/dev/fb0    

export FB_FRAMEBUFFER_0=/dev/fb0    

export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1   

export QT_QPA_PLATFORM=eglfs   

/home/root/bin/test

root@imx6qsabreauto:~# cat /home/root/bin/lvds.sh

#!/bin/sh

export QT_QPA_EGLFS_FB=/dev/fb4

export FB_FRAMEBUFFER_0=/dev/fb4

export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1

export QT_QPA_PLATFORM=eglfs

/home/root/bin/test

is it normal or can be fixed?

0 Kudos
Reply
1 Reply

931 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrey

p.6 below presentation shows max. two video performance

without os

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

it may be less based on bus load and application

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------