Unable to update KDS from 3.0.0 to 3.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to update KDS from 3.0.0 to 3.1.0

Jump to solution
4,992 Views
gorakk
Contributor IV

When attempting to install Kinetis Design Studio 3.1.0 the installer says that the operation cannot be completed and gives these details:

 

Cannot complete the install because one or more required items could not be found.

  Software currently installed: GNU ARM C/C++ J-Link Debugging 3.2.1.201508190739 (ilg.gnuarmeclipse.debug.gdbjtag.jlink.feature.group 3.2.1.201508190739)

  Missing requirement: GNU ARM C/C++ J-Link Debugging 3.2.1.201508190739 (ilg.gnuarmeclipse.debug.gdbjtag.jlink.feature.group 3.2.1.201508190739) requires 'ilg.gnuarmeclipse.debug.gdbjtag [2.2.1.201508190739]' but it could not be found

 

 

Does anyone know of a way to fix this? 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
4,560 Views
BlackNight
NXP Employee
NXP Employee

Hi Allen,

yes, maybe doing this from a clean install is the easiest way. You should not need to uninstall it first: rename your original installation folder and then install it again. I recommend that you do a zip archive of the 'clean' installation folder so you can go easily back to it if something fails.

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
8 Replies
4,560 Views
marcinmazur
Contributor II

Please check solution to my problem here: https://community.freescale.com/thread/387164#comment-624040

0 Kudos
Reply
4,560 Views
michals
Contributor II

I have the same problem but with a different error message. This error is for Windows 7 install and update. I can update correctly 3.0 -> 3.1 under Linux.

An error occurred while uninstalling

session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Uninstall, operand=[R]com.somniumtech.kds.executable.win32.win32.x86 3.0.0 --> null, action=org.eclipse.equinox.internal.p2.touchpoint.natives.actions.CleanupzipAction).

Backup of file D:\nxp\KDS_3.0.0\eclipse\kinetis-design-studio.exe failed.

File that was copied to backup could not be deleted: D:\nxp\KDS_3.0.0\eclipse\kinetis-design-studio.exe

0 Kudos
Reply
4,560 Views
BlackNight
NXP Employee
NXP Employee

Hi michals,

could it that you had another instance of KDS running? Make sure there is only one KDS running while you do the update.

I hope this helps,

Erich

0 Kudos
Reply
4,560 Views
BlackNight
NXP Employee
NXP Employee

Hi Allen,

Somehow the dependencies are not properly resolved. Could you try with these settings:

pastedImage_0.png

I hope this helps,

Erich

0 Kudos
Reply
4,560 Views
BlackNight
NXP Employee
NXP Employee

Additionally, you might update the GNU ARM Eclipse plugins. Below is what I have (after updating to 3.1.0):

gnu arm.png

Erich

0 Kudos
Reply
4,559 Views
gorakk
Contributor IV

Hi Erich,

Thanks for looking into this!

I tried the first suggestion and there was no change - still got the same error.

After updating the GNU ARM Eclipse plugins - attempting to install the 3.1.0 update gave this error:

An error occurred while collecting items to be installed

session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

No repository found containing: osgi.bundle,com.somniumtech.branding.kds,3.1.0.201512141710

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.debug.gdbjtag,2.2.2.201512141335

No repository found containing: osgi.bundle,ilg.gnuarmeclipse.managedbuild.cross,2.1.1.201512141335

No repository found containing: org.eclipse.update.feature,com.somniumtech.kds.doc.releasenotes,3.1.0.201512141710

No repository found containing: binary,com.somniumtech.kds.executable.win32.win32.x86,3.1.0.201512141710

No repository found containing: org.eclipse.update.feature,com.somniumtech.kds,3.1.0.201512141710

Is the best course of action at this point just uninstalling / reinstalling KDS?

Allen

0 Kudos
Reply
4,561 Views
BlackNight
NXP Employee
NXP Employee

Hi Allen,

yes, maybe doing this from a clean install is the easiest way. You should not need to uninstall it first: rename your original installation folder and then install it again. I recommend that you do a zip archive of the 'clean' installation folder so you can go easily back to it if something fails.

I hope this helps,

Erich

0 Kudos
Reply
4,561 Views
gorakk
Contributor IV

Erich,

That did the trick - I renamed the KDS_3.0.0 directory and then ran the installer.  When the installer prompted for Modify, Repair, or Remove I selected Repair.

After the installation was complete I used the Install New Software function to first install the update to 3.1 and then installed updates for other items.

Thanks!

Allen

0 Kudos
Reply