Hi,
I am using IMX6SL EVK with 3G USB dongle (Huawei-EM770) in Android Kitkat 4.4.2 ( kernel version 3.0.35).
When i insert the Huawei-EM770 3G USB dongle, the minicom shows like below lines:
root@evk_6sl:/ # usb 1-1: new high speed USB device number 9 using fsl-ehci
usb 1-1: device v0685 p7000 is not supported
scsi18 : usb-storage 1-1:1.0
scsi 18:0:0:0: CD-ROM 3G USB MMC Storage 2.31 PQ: 0 ANSI: 2
scsi 18:0:0:1: Direct-Access 3G USB MMC Storage 2.31 PQ: 0 ANSI: 2
sd 18:0:0:1: [sda] Attached SCSI removable disk
type=1400 audit(87704.270:30): avc: denied { setgid } for pid=3565 comm="ntfs-3g" capability=6 scontext=u:r:vold:s0 tcontext=u:y
type=1400 audit(87704.300:31): avc: denied { setuid } for pid=3565 comm="ntfs-3g" capability=7 scontext=u:r:vold:s0 tcontext=u:y
type=1400 audit(87704.330:32): avc: denied { getattr } for pid=3565 comm="ntfs-3g" path="/dev/fuse" dev=tmpfs ino=743 scontext=ue
type=1400 audit(87704.360:33): avc: denied { setgid } for pid=3565 comm="ntfs-3g" capability=6 scontext=u:r:vold:s0 tcontext=u:y
type=1400 audit(87704.380:34): avc: denied { setuid } for pid=3565 comm="ntfs-3g" capability=7 scontext=u:r:vold:s0 tcontext=u:y
init: no such service 'fuse_udisk'
usb 1-1: USB disconnect, device number 9
usb 1-1: new high speed USB device number 10 using fsl-ehci
usb 1-1: device v12d1 p1001 is not supported
option 1-1:1.0: GSM modem (1-port) converter detected
usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0
option 1-1:1.1: GSM modem (1-port) converter detected
usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1
option 1-1:1.2: GSM modem (1-port) converter detected
usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2
option 1-1:1.3: GSM modem (1-port) converter detected
usb 1-1: GSM modem (1-port) converter now attached to ttyUSB3
scsi23 : usb-storage 1-1:1.4
scsi 23:0:0:0: CD-ROM 3G USB MMC Storage 2.31 PQ: 0 ANSI: 2
scsi 23:0:0:1: Direct-Access 3G USB MMC Storage 2.31 PQ: 0 ANSI: 2
sd 23:0:0:1: [sda] Attached SCSI removable disk
type=1400 audit(87735.270:35): avc: denied { setgid } for pid=3618 comm="ntfs-3g" capability=6 scontext=u:r:vold:s0 tcontext=u:y
type=1400 audit(87735.300:36): avc: denied { setuid } for pid=3618 comm="ntfs-3g" capability=7 scontext=u:r:vold:s0 tcontext=u:y
type=1400 audit(87735.330:37): avc: denied { getattr } for pid=3618 comm="ntfs-3g" path="/dev/fuse" dev=tmpfs ino=743 scontext=ue
type=1400 audit(87735.360:38): avc: denied { setgid } for pid=3618 comm="ntfs-3g" capability=6 scontext=u:r:vold:s0 tcontext=u:y
type=1400 audit(87735.390:39): avc: denied { setuid } for pid=3618 comm="ntfs-3g" capability=7 scontext=u:r:vold:s0 tcontext=u:y
init: no such service 'fuse_udisk'
Display shows the network signal .But netwok signal is weak . If i enable the Data enabled option in Android Settings. The network signal is lost.
Huawei-EM770 3G USB dongle cannot work properly.
I attached the logcat file for radio interface .Please find it . Give any suggestion to make Huawei-EM770 3G USB dongle work in IMX6SL EVK in Android platform.
Regards,
vinothraj
Original Attachment has been moved to: test.txt.zip