IMX6SL EVK with 3G USB dongle (Huawei-EM770)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SL EVK with 3G USB dongle (Huawei-EM770)

870 Views
vinothrajm
Contributor III

Hi,

 

I am using IMX6SL EVK with 3G USB dongle (Huawei-EM770) in Android Kitkat 4.4.2 ( kernel version 3.0.35).

 

When i insert the Huawei-EM770 3G USB dongle, the minicom shows like below lines:

 

root@evk_6sl:/ # usb 1-1: new high speed USB device number 9 using fsl-ehci

usb 1-1: device v0685 p7000 is not supported

scsi18 : usb-storage 1-1:1.0

scsi 18:0:0:0: CD-ROM            3G USB   MMC Storage      2.31 PQ: 0 ANSI: 2

scsi 18:0:0:1: Direct-Access     3G USB   MMC Storage      2.31 PQ: 0 ANSI: 2

sd 18:0:0:1: [sda] Attached SCSI removable disk

type=1400 audit(87704.270:30): avc:  denied  { setgid } for  pid=3565 comm="ntfs-3g" capability=6  scontext=u:r:vold:s0 tcontext=u:y

type=1400 audit(87704.300:31): avc:  denied  { setuid } for  pid=3565 comm="ntfs-3g" capability=7  scontext=u:r:vold:s0 tcontext=u:y

type=1400 audit(87704.330:32): avc:  denied  { getattr } for  pid=3565 comm="ntfs-3g" path="/dev/fuse" dev=tmpfs ino=743 scontext=ue

type=1400 audit(87704.360:33): avc:  denied  { setgid } for  pid=3565 comm="ntfs-3g" capability=6  scontext=u:r:vold:s0 tcontext=u:y

type=1400 audit(87704.380:34): avc:  denied  { setuid } for  pid=3565 comm="ntfs-3g" capability=7  scontext=u:r:vold:s0 tcontext=u:y

init: no such service 'fuse_udisk'

usb 1-1: USB disconnect, device number 9

usb 1-1: new high speed USB device number 10 using fsl-ehci

usb 1-1: device v12d1 p1001 is not supported

option 1-1:1.0: GSM modem (1-port) converter detected

usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0

option 1-1:1.1: GSM modem (1-port) converter detected

usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1

option 1-1:1.2: GSM modem (1-port) converter detected

usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2

option 1-1:1.3: GSM modem (1-port) converter detected

usb 1-1: GSM modem (1-port) converter now attached to ttyUSB3

scsi23 : usb-storage 1-1:1.4

scsi 23:0:0:0: CD-ROM            3G USB   MMC Storage      2.31 PQ: 0 ANSI: 2

scsi 23:0:0:1: Direct-Access     3G USB   MMC Storage      2.31 PQ: 0 ANSI: 2

sd 23:0:0:1: [sda] Attached SCSI removable disk

type=1400 audit(87735.270:35): avc:  denied  { setgid } for  pid=3618 comm="ntfs-3g" capability=6  scontext=u:r:vold:s0 tcontext=u:y

type=1400 audit(87735.300:36): avc:  denied  { setuid } for  pid=3618 comm="ntfs-3g" capability=7  scontext=u:r:vold:s0 tcontext=u:y

type=1400 audit(87735.330:37): avc:  denied  { getattr } for  pid=3618 comm="ntfs-3g" path="/dev/fuse" dev=tmpfs ino=743 scontext=ue

type=1400 audit(87735.360:38): avc:  denied  { setgid } for  pid=3618 comm="ntfs-3g" capability=6  scontext=u:r:vold:s0 tcontext=u:y

type=1400 audit(87735.390:39): avc:  denied  { setuid } for  pid=3618 comm="ntfs-3g" capability=7  scontext=u:r:vold:s0 tcontext=u:y

init: no such service 'fuse_udisk'

 

Display shows the network signal .But netwok signal is weak . If i enable the Data enabled option in Android Settings. The network signal is lost.

Huawei-EM770 3G USB dongle cannot work properly.

 

I attached the logcat file for radio interface .Please find it . Give any suggestion to make Huawei-EM770 3G USB dongle work in IMX6SL EVK in Android platform.

 

 

 

Regards,

vinothraj

Original Attachment has been moved to: test.txt.zip

Labels (2)
0 Kudos
1 Reply

508 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi vinothraj,

     see the document : Gudielines on 3G modem integration

     In addition, if linux system can't recognatize USB modem, you can add PID & VID to file options.c in usb driver.

Regards,

Weidong

0 Kudos