Monochrome camera support in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Monochrome camera support in i.MX6

Jump to solution
2,024 Views
ko-hey
Senior Contributor II

Hi all

I have a question for using monochrome camera.

My customer are planning to use i.MX6Dual or DualLite and monochrome camera of MT9V024 series.

"MT9V024 series Datasheet"

file:///C:/Users/110719/Downloads/MT9V024_Flyer.pdf

In Reference manual, i.MX6's parallel interface supports Gray Scale. This means we can use monochrome camera. Is it correct?

If yes, please tell me how to connect it to i.MX6 and the notes of using a monochrome camera.

Also does Linux driver support a monochrome camera?

Please tell me.

Best Regards,

Labels (3)
0 Kudos
Reply
1 Solution
1,454 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

yes i.MX6DQ, SDL supports monochrome camera (bayer format), connection

is the same as other cameras, it is not supported in BSP however one

can find many Community links for its support

https://community.freescale.com/message/331888

https://community.freescale.com/message/309833#309833

https://community.freescale.com/message/309069#309069

Re: IPU - bayer pattern conversion

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,455 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

yes i.MX6DQ, SDL supports monochrome camera (bayer format), connection

is the same as other cameras, it is not supported in BSP however one

can find many Community links for its support

https://community.freescale.com/message/331888

https://community.freescale.com/message/309833#309833

https://community.freescale.com/message/309069#309069

Re: IPU - bayer pattern conversion

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,454 Views
ko-hey
Senior Contributor II

Igor

Thank you!

I understood that we can use monochrome camera and need BSP customization.

ko-hey

0 Kudos
Reply