K60 UART interrupt is stuck

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 UART interrupt is stuck

2,743 Views
gerry26
Contributor I

Hi,

My UART interface RX stream is stuck and no new RX interrupt  is received for any attempt to drive input.

I experience a UART overflow, caused by interrupt long latency, which leaves the system with no active interrupt but with a char in the buffer.

This prevents from new char to be received. the only thing that "releases" the UART interface is D read.

Following this read the interface is released and the RX flow runs once again.

The UART statuses doesn't apply to any reasonable cause.

See UART status log below:

4006A000: 00 36 00 2C C8 40 00 XX 00 00 08 00 00 00 00 AA

4006A010: 22 00 C5 00 00 01 00 AA 00 00 00 0A 00 01 00 00

4006A020: AA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

4006A030: 00 00 AA AA AA AA AA AA AA AA

Please note that the XX located in 4006A007 is the D register. Once this address is called the block is released.

Tnx,

Gerry

Tags (3)
0 Kudos
Reply
1 Reply

2,218 Views
mjbcswitzerland
Specialist V

Gerry

When an overrun takes place the overrun flag must be correctly cleared otherwise the UART receiver will not process further reception.

Please see the following with explanation of how to reset it (towards the end of the thread): Lost UART interrupt on MK60DN512xxx10

Regards

Mark

0 Kudos
Reply