Question, i.MX6SoloLite EVK/Android touch screen support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6SoloLite EVK/Android touch screen support

Jump to solution
2,782 Views
Aemj
Contributor IV

Hi All,

I would like to ask about the feature of android BSP(JB4.3_1.1.0) on i.MX6 SoloLite EVK.

In Android Release Note attached in your android bsp(JB4.3_1.1.0), it is said that UI input is not supported on i.MX6SoloLite EVK.

When using MCIMX28LCD with i.MX6SoloLite EVK, doesn’t the touch screen work with your AndroidBSP?

Could you show me how I can do for the touch screen to work?

BR,

Miyamoto

Labels (2)
0 Kudos
Reply
1 Solution
2,432 Views
PeterChan
NXP Employee
NXP Employee

Hi Miyamoto,

The touch panel on MCIMX28LCD does not work in i.MX6SoloLite EVK. You have to plug a USB mouse to the USB host port of the i.MX6SoloLite EVK to enable the user input.

View solution in original post

0 Kudos
Reply
2 Replies
2,433 Views
PeterChan
NXP Employee
NXP Employee

Hi Miyamoto,

The touch panel on MCIMX28LCD does not work in i.MX6SoloLite EVK. You have to plug a USB mouse to the USB host port of the i.MX6SoloLite EVK to enable the user input.

0 Kudos
Reply
2,432 Views
Aemj
Contributor IV

Hi,

Does anyone know how to make it work?

0 Kudos
Reply