Which type IBIS model should I select using with industrial i.MX6DL ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which type IBIS model should I select using with industrial i.MX6DL ?

Jump to solution
2,855 Views
koichisakagami
Contributor II

Dear Sirs ,

I have one question.

There are two  IBIS model type ( for consumer and for automotive ) on FS web site.

I use the industrial i.MX6DL.

Which type IBIS model should I use ?

Best Regards,

Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
2,539 Views
SergioSolis
NXP Employee
NXP Employee

You should use the automotive version

View solution in original post

0 Kudos
Reply
6 Replies
2,539 Views
SergioSolis
NXP Employee
NXP Employee

Hello Koichi,

Both files are actually the same file (renamed differently), so you can choose any.

0 Kudos
Reply
2,539 Views
i_chee
Contributor I

@SerchMX Using any of the files causes my installation of Hyperlynx to crash when selecting any of the DRAM pins. All other pins work as intended but selecting any DRAM pin causes immediate crash. How can I fix this? I haven't had any problems with other ibis files. Only changes I've had to make to this ibis file is commenting 6 lines that pair differential pins which aren't connected. For the record, I've tried both consmr and autmtv version.

|D1          D2       NA        NA        NA        NA

|E3          E4       NA        NA        NA        NA

|F3          F4       NA        NA        NA        NA

|G1          G2       NA        NA        NA        NA

|H1          H2       NA        NA        NA        NA

|H3          H4       NA        NA        NA        NA

0 Kudos
Reply
2,539 Views
koichisakagami
Contributor II

Dear SerchMX san,

I checked the two IBIS Model difference about

mx6sdl_21x21_autmtv_v1_4.ibs and mx6sdl_21x21_consmr_v1_4.ibs.

It is not same.

Could you tell me which type IBIS model should I use ?

Best Regards,

Koichi Sakagami

0 Kudos
Reply
2,540 Views
SergioSolis
NXP Employee
NXP Employee

You should use the automotive version

0 Kudos
Reply
2,539 Views
koichisakagami
Contributor II

Dear SerchMX san,

Thank you for your answer.

Best Regards,

Koichi Sakagami

0 Kudos
Reply
2,539 Views
koichisakagami
Contributor II

Dear SerchMX san,

Thank you for reply.
I got it.

Best Regards,

Koichi Sakagami

0 Kudos
Reply