Which type IBIS model should I select using with industrial i.MX6DL ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which type IBIS model should I select using with industrial i.MX6DL ?

跳至解决方案
2,756 次查看
koichisakagami
Contributor II

Dear Sirs ,

I have one question.

There are two  IBIS model type ( for consumer and for automotive ) on FS web site.

I use the industrial i.MX6DL.

Which type IBIS model should I use ?

Best Regards,

Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
2,440 次查看
SergioSolis
NXP Employee
NXP Employee

You should use the automotive version

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,440 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Koichi,

Both files are actually the same file (renamed differently), so you can choose any.

0 项奖励
回复
2,440 次查看
i_chee
Contributor I

@SerchMX Using any of the files causes my installation of Hyperlynx to crash when selecting any of the DRAM pins. All other pins work as intended but selecting any DRAM pin causes immediate crash. How can I fix this? I haven't had any problems with other ibis files. Only changes I've had to make to this ibis file is commenting 6 lines that pair differential pins which aren't connected. For the record, I've tried both consmr and autmtv version.

|D1          D2       NA        NA        NA        NA

|E3          E4       NA        NA        NA        NA

|F3          F4       NA        NA        NA        NA

|G1          G2       NA        NA        NA        NA

|H1          H2       NA        NA        NA        NA

|H3          H4       NA        NA        NA        NA

0 项奖励
回复
2,440 次查看
koichisakagami
Contributor II

Dear SerchMX san,

I checked the two IBIS Model difference about

mx6sdl_21x21_autmtv_v1_4.ibs and mx6sdl_21x21_consmr_v1_4.ibs.

It is not same.

Could you tell me which type IBIS model should I use ?

Best Regards,

Koichi Sakagami

0 项奖励
回复
2,441 次查看
SergioSolis
NXP Employee
NXP Employee

You should use the automotive version

0 项奖励
回复
2,440 次查看
koichisakagami
Contributor II

Dear SerchMX san,

Thank you for your answer.

Best Regards,

Koichi Sakagami

0 项奖励
回复
2,440 次查看
koichisakagami
Contributor II

Dear SerchMX san,

Thank you for reply.
I got it.

Best Regards,

Koichi Sakagami

0 项奖励
回复