HAB secure serial boot on mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HAB secure serial boot on mx6

Jump to solution
5,671 Views
mmeuli
Contributor I

Hello

I am working on HAB secure boot. We can boot secure from NAND and MMC using boards in open and closed configuration.

However I have not managed to boot via freescale manufacturing tools without HAB events.

If we boot a 'normal' singed u-boot.bin via MFG tool, we get ~5 HAB events.

If we use the scripts from AN4581 6.2, I still get one single HAB event.

--------- HAB Event 1 -----------------

event data:

  0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

  0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00

  0x00 0x00 0x02 0x88

  STS: 0x33 RSN: 0x0c CTX: 0xa0 ENG: 0x00

Does anyone have experience with secure serial boot?

What irritates me, is that we had to remove the coma / logical line break from the sample cst code in AN4581. The sample in AN 4581 generates a syntax error.

[Authenticate Data]

Verification index = 2

Blocks = 0x10800400 0x400 0x2BC00 "u-boot-pad.bin", \

Blocks = 0x00910000 0x430 0x2E0 "u-boot-pad.bin"

How do I get rid of that HAB event?

Regards,

  Martin

Labels (1)
0 Kudos
Reply
1 Solution
3,594 Views
Yuri
NXP Employee
NXP Employee

1.

As I know the problem was solved :

From AN 4581:

--

[Authenticate Data]

Verification index = 2

Blocks = 0x10800400 0x400 0x2BC00 "u-boot-pad.bin", \ Blocks = 0x00910000 0x430 0x2E0 "u-boot-pad.bin"

--

This generates a syntax error

We used:

--

[Authenticate Data]

        Verification index = 2

        Blocks = 0x27800400 0x400 0x3BC00 "u-boot-pad.bin"

        Blocks = 0x00910000 0x42c 0x288 "u-boot-pad.bin"

--

This generates a HAB assert at 0x00910000

--

[Authenticate Data]

        Verification index = 2

        Blocks = 0x00910000 0x42c 0x288 "u-boot-pad.bin"

        Blocks = 0x27800400 0x400 0x3BC00 "u-boot-pad.bin"

--

Generates 3 HAB assertions in DRAM

--

[Authenticate Data]

        Verification index = 2

        Blocks = 0x00910000 0x42c 0x288 "u-boot-pad.bin"

[Authenticate Data]

        Verification index = 2

        Blocks = 0x27800400 0x400 0x3BC00 "u-boot-pad.bin"

--

This works.

2.

As for the HAB Event below :

--------- HAB Event 1 -----------------

event data:

  0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

  0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00

  0x00 0x00 0x02 0x88

  STS: 0x33 RSN: 0x0c CTX: 0xa0 ENG: 0x00

Header Word: 0xdb 0x00 0x14 0x41

Tag = 0xDB Event

Length = 0x0014 Length of event record in bytes

Version: 0x41 HAB Version

SRCE Word: 0x33 0x0c 0xa0 0x00

Status = 0x33 HAB_FAILURE

Reason = 0x0c HAB_INV_ASSERTION

Context = 0xa0 HAB_CTX_AUTHENTICATE

Engine = 0x00 HAB_ENG_ANY

Event Data: Since the Context is HAB_CTX_AUTHENTICATE the reason must also be

taken into account.

Here the reason is HAB_INV_ASSERTION so the context dependent data in this

example corresponds to HAB_CTX_ASSERT which contains the hab_rvt.assert() call

parameters in the order they appear in the parameter list.

type: 0x00 0x00 0x00 0x00 = HAB_ASSERT_BLOCK

0x00 0x91 0x00 0x00 = data address

0x00 0x00 0x02 0x88 = data length in bytes

Note, that the API checks that all of the following data have been authenticated

(using their final locations):

IVT

DCD (if provided);

Boot Data (initial byte if provided);

Entry point (initial word).

Each of the above data components not covered by a valid signature will cause

HAB to generate an event with reason HAB_INV_ASSERTION like the one above.

View solution in original post

0 Kudos
Reply
2 Replies
3,594 Views
torenyan
Contributor I

Hello Martin,sorry to bother u.but hope you can do me a favor with "Signing Code Downloadable with Manufacturing Tool".

I've done as the AN4581 says.but i met HAB Event unfortunately.witch as follow.

Out:   serial

Err:   serial

Checking HAB_status

HAB Configuration: 0xf0  HAB State: 0x66

--------- HAB Event 1 -----------------

event data:

    0xdb 0x00 0x08 0x41 0x33 0x22 0x0a 0x00

--------- HAB Event 2 -----------------

event data:

    0xdb 0x00 0x08 0x41 0x33 0x22 0x0a 0x00

--------- HAB Event 3 -----------------

event data:

    0xdb 0x00 0x08 0x41 0x33 0x22 0x0a 0x00

--------- HAB Event 4 -----------------

event data:

    0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

    0x00 0x00 0x00 0x00 0x27 0x80 0x07 0x00

    0x00 0x00 0x00 0x20

--------- HAB Event 5 -----------------

event data:

    0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

    0x00 0x00 0x00 0x00 0x27 0x80 0x07 0x20

    0x00 0x00 0x00 0x04

--------- HAB Event 6 -----------------

event data:

    0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

    0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00

    0x00 0x00 0x02 0xe0

Net:   got MAC address from IIM: 00:01:02:03:04:05

FEC0 [PRIME]

..main_loop

------------------------------------------------------------------------------------------------------

My u-boot.csf file comes bellow:

-----------------------------------------------------------------------------------------------------

[Header]

  Version = 4.0

  Security Configuration = Open

  Hash Algorithm = sha256

  Engine Configuration = 0

  Certificate Format = X509

  Signature Format = CMS

[Install SRK]

  File = "../crts/SRK_1_2_3_4_table.bin"

  Source index = 0

[Install CSFK]

  File = "../crts/CSF1_1_sha256_1024_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]

  Verification index = 0

  Target index = 2

  File = "../crts/IMG1_1_sha256_1024_65537_v3_usr_crt.pem"

# Sign padded u-boot starting at the IVT through to the end with

# length = 0x2F000 (padded u-boot length) - 0x400 (IVT offset) = 0x2EC00

# Note: 0x2F000 may be different depending on the size of U-Boot

# This covers the essential parts: IVT, boot data and DCD.

# Blocks have the following definition:

# Image block start address on i.MX, Offset from start of image file,

# Length of block in bytes, image data file

[Authenticate Data]

  Verification index = 2

  Blocks = 0x27800400 0x400 0x2EC00 "u-boot-pad.bin",\

    0x00910000 0x42C 0x2E0 "u-boot-pad.bin"

---------------------------------------------------------------------------------------------------

QQ图片20140322124824.jpg

The pic above is the IVT get from u-boot-signed-pad.bin.

--------------------------------------------------------------------------------------------------

Can u help me with this.TKS.

0 Kudos
Reply
3,595 Views
Yuri
NXP Employee
NXP Employee

1.

As I know the problem was solved :

From AN 4581:

--

[Authenticate Data]

Verification index = 2

Blocks = 0x10800400 0x400 0x2BC00 "u-boot-pad.bin", \ Blocks = 0x00910000 0x430 0x2E0 "u-boot-pad.bin"

--

This generates a syntax error

We used:

--

[Authenticate Data]

        Verification index = 2

        Blocks = 0x27800400 0x400 0x3BC00 "u-boot-pad.bin"

        Blocks = 0x00910000 0x42c 0x288 "u-boot-pad.bin"

--

This generates a HAB assert at 0x00910000

--

[Authenticate Data]

        Verification index = 2

        Blocks = 0x00910000 0x42c 0x288 "u-boot-pad.bin"

        Blocks = 0x27800400 0x400 0x3BC00 "u-boot-pad.bin"

--

Generates 3 HAB assertions in DRAM

--

[Authenticate Data]

        Verification index = 2

        Blocks = 0x00910000 0x42c 0x288 "u-boot-pad.bin"

[Authenticate Data]

        Verification index = 2

        Blocks = 0x27800400 0x400 0x3BC00 "u-boot-pad.bin"

--

This works.

2.

As for the HAB Event below :

--------- HAB Event 1 -----------------

event data:

  0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

  0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00

  0x00 0x00 0x02 0x88

  STS: 0x33 RSN: 0x0c CTX: 0xa0 ENG: 0x00

Header Word: 0xdb 0x00 0x14 0x41

Tag = 0xDB Event

Length = 0x0014 Length of event record in bytes

Version: 0x41 HAB Version

SRCE Word: 0x33 0x0c 0xa0 0x00

Status = 0x33 HAB_FAILURE

Reason = 0x0c HAB_INV_ASSERTION

Context = 0xa0 HAB_CTX_AUTHENTICATE

Engine = 0x00 HAB_ENG_ANY

Event Data: Since the Context is HAB_CTX_AUTHENTICATE the reason must also be

taken into account.

Here the reason is HAB_INV_ASSERTION so the context dependent data in this

example corresponds to HAB_CTX_ASSERT which contains the hab_rvt.assert() call

parameters in the order they appear in the parameter list.

type: 0x00 0x00 0x00 0x00 = HAB_ASSERT_BLOCK

0x00 0x91 0x00 0x00 = data address

0x00 0x00 0x02 0x88 = data length in bytes

Note, that the API checks that all of the following data have been authenticated

(using their final locations):

IVT

DCD (if provided);

Boot Data (initial byte if provided);

Entry point (initial word).

Each of the above data components not covered by a valid signature will cause

HAB to generate an event with reason HAB_INV_ASSERTION like the one above.

0 Kudos
Reply